This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: Unable to access Debug Properties in CCS Theia

Part Number: MSP432E401Y

Tool/software:

I currently can't access the Debug-Properties in the CCS Theia, Version 20.2.0.12_1.8.0, as there is the Error "Cannot read properties of undefined (reading 'name')". Reason for trying to access the Debug-Settings is, that I only want to set the Erase Config to the only required segments.

I'm using a Segger J-Link Debugger to connect via SWD to a custom board with an MSP432E401Y.

Is there any way to set the Erase-Config with the J-Link on the new CCS Theia? In the Eclipse based version it was possible and I havely used this function.

Thanks