Part Number: MSPM0C1104
Tool/software:
Hi,
I'm designing a small application that uses the 8 pin version but I cannot leave debug pins assigned, so once programmed as require they
don't allow further reprogramming.
Is there an easy way to restore original (debug) pin configuration from the application? i.e. a user command from serial line?
question 2:
is there an easy way to store in flash a few configuration parameter that do not require often updates? I would avoid the
quite complex e2prom emulation, changes per location less than 100..
thanks