Part Number: LP-AM261
Tool/software:
Hi!
I have been developing/debugging an application on the PRU the following way:.
1 Load my FreeRTOS application on R5_0 via jtag
2 Halted R5_0 at AppMain() in freertos_main()
3 Attached to ICSSM1_PRU_1 and loaded my pru.out application via CCS
And that has worked fine for me, but now I need to switch over to loading the PRU application programmatically via PRUICSS_loadFirmware() and I just can't get it to work.
I have enabled the "PRU hex utility" and the output format is Array (--array) but maybe there are some other settings that I need to configure? And is it possible to step trough the code when you load it with PRUICSS_loadFirmware just like when you load the application manually via CCS?
Best regards
Daniel