Part Number: LP-AM261
Tool/software:
Dear TI Support Team,
I am working with the LP-AM261 and its PROFINET stack as provided in the SDK ind_comms_sdk_am261x_10_02_00_05. I have a question regarding the handling of the "Delayed Application Ready" mechanism in the PROFINET implementation.
Does the PROFINET stack support delaying the Application Ready signal from the device to the IO-Controller?
My use case involves receiving configuration data via Write Record, then processing the Parameter End indication. After that, the application performs internal setup, such as configuring the underlying network interfaces or devices.
-
If an error occurs during this setup phase, is there a way for the application to indicate an error back to the IO-Controller, before signaling Application Ready? (e.g set the erroneous submodules to "ApplicationReady pending" )
-
Additionally, is it possible for the application to explicitly send the Application Ready signal once the internal setup completes successfully?
I would appreciate any clarification on whether this flow is supported by the stack?
Best Regards
J.Zribi