This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L2227: Does clock accuracy improve when the operating temperature range is narrow?

Genius 3215 points

Part Number: MSPM0L2227

Tool/software:

Hi All,

When using M0 in the range of 5 to 40°C,
will the MIN and MAX values of SYSOSC accuracy improve?

We expect the accuracy at 5 to 40°C to be better than the accuracy at -40 to 85°C.

Best Regards,

Ito