This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM273X: SPI development

Part Number: MCU-PLUS-SDK-AM273X
Other Parts Discussed in Thread: LMX2595

Tool/software:

Hello Support team,

To develop a SPI project, what sample project should I start with? Or should I start from an empty sample project?

I also find there are SPI and QSPI. Which one should I choose from?

Best regards,

  • Hi Lin,

    You can start the SPI project with either

    C:\ti\mcu_plus_sdk_am273x_09_02_00_60\examples\drivers\mibspi\mibspi_loopback or

    C:\ti\mcu_plus_sdk_am273x_09_02_00_60\examples\drivers\mibspi\mibspi_loopback_dma depending on which mode you want to use: CPU copy or DMA copy assuming you want to use the SPI to transmit data.

    The QSPI is for the flash read/write.

    Best regards,

    Ming

  • Hi Ming,

    Thank you very much for your reply. And I'm glad you are responsible to my new post again.

    What's the difference between mibspi and standard spi? Can I set mibspi to standard spi?

    Also, I have import and built the sample project mibspi_loopback_r5fss0-0_nortos. Now I plan to modify the mibspi to connect with external device with standard spi. Set AM273x in master spi mode and assign physical pins to the EVM headers. How should I do them? 

    I plan to start from .syscfg file. Is it a good way to start from? If yes, how should I do? Could you provide some detailed instructions with screenshots?

    Appreciate your help and support.

    Best regards,

    Lin

  • Hi Lin,

    Multi-Buffered Serial Peripheral Interface Module (MibSPI) is a TI version of SPI. It has two modes:

    The Multi-buffer Mode and Compatible Mode. The compatible mode is the same as the SPI.

    Yes. You should start with the example.syscfg file of sample project mibspi_loopback_r5fss0-0_nortos:

    As you can see, you will need to configure the SPI interface like, SPI frequency, 3 or 4 pin mode, pins for SPI CLK, MISO, MOSI and CS, master or slave etc.

    Then in the program mibspi_loopback.c, you will need to comment out the call to MIBSPI_enableLoopback(), because it will enable the loopback mode (whatever comes out of TX will goes to RX).

    Best regards,

    Ming

  • Hi Ming,

    Thanks for your instructions. I am working on the example.syscfg. I have two questions.

    - Can I disable loopback mode in the example.syscfg? Or I can only do it in the code.

    - For the Pin Assignment, the current setting is:

    MIBSPI CLK Pin(MSS_MIBSPIA_CLK) PAD_DJ/G19 with Pull Up
    MIBSPI MISO Pin(MSS_MIBSPIA_MISO) PAD_DI/G17 with Pull Up
    MIBSPI MOSI Pin(MSS_MIBSPIA_MOSI) PAD_DH/H18 with Pull Up

    CS Pin PAD_DK/F19 No Pull

    How can I measure/test those 4 pins signals on the EVM board?

    Best regards,

    Lin

  • Hi Ming,

    Could you point me to the EVM board schematics file?

    Thanks,

    Lin

  • Hi Lin,

    Please check the following URL: 

    AM273x Evaluation Module User's Guide (Rev. D)

    You can also find the design file package in: https://www.ti.com/lit/zip/sprr504.

    Best regards,

    Ming

  • Hi Ming,

    Thanks for your help and links to the documents. I will study them and get back to you later.

    Regards,

    Lin

  • Hi Ming,

    After carefully reading the EVM User Guide, especially the section 2.2.9 SPI Interface, I notice that there are four SPI choices:

    - MSS_SPIA is wired to FTDI USB port (J10). However, I'm not sure how I can test the 4 pin signals of MSS_SPIA on J10.

    - MSS_SPIB can be multiplexed and connected to J16 by setting S2 to PMIC_SPI position. Also the R5, R61, R167 and R176 need to be populated with 0 ohm (by checking the S2 part and BOM of EVM). Do you think MSS_SPIB to J16 is a good choice? If so, I need to add 4 resistors on the EVM board and modify the example.syscfg file to MSS_SPIB. Please give your comments.

    - RCSS_SPIA routed to J1 (60 pin connector), it's hard to get the SPI signals.

    - RCSS_SPIB routed to J11 (60 pin connector), it's hard to get the SPI signals.

    Could you provide your advice before I go ahead further? If you could explain your choice, that would be great.

    Best regards,

    Lin

  • Hi Lin,

    What we did is to use the 60-pin breakout adapter (ZX100-QTH030-ST Samtec Breakout Adapter) and plug it into the 60-pin connector on AM273x EVM, then we use Saleae Logic Pro to capture the SPI signals.

    Best regards,

    Ming

  • Hi Ming,

    Do you mean you will use RCSS_SPIA or RCSS_SPIB and get signal from the 60-pin connector with the adapter? How about the MSS_SPIA or MSS_SPIB?

    Thanks,
    Lin

  • Hi Ming,

    Oh, MSS_SPIB can be connected to J7 60-pin connector too. 

    Could you describe your choice and setting in more detail?

    Best regards,

    Lin

  • Hi Lin,

    It depends on which core are you using. If you run your program on R5F_0, then MSS_SPIA can be used. If you are using the C66x core, then only RCSS_SPIA can be used.

    Best regards,

    Ming

  • Hi Ming,

    Thanks. I didn't have that idea. Now clear.

    If we choose MSS_SPIA, do we need to use the 60-pin breakout adapter (ZX100-QTH030-ST Samtec Breakout Adapter)? 

    Regards,

    Lin

  • Hi Lin,

    According to schematics, the J16 can connect to MSS_SPIB, but you will need to populate 4 0ohm resistors, then you do not need the adaptor.

    MSS_SPIA goes to the FTDI chip. I do not see an easy way to measure it.

    RCSS_SPIA and RCSS_SPIB are connected to the 60-pin connectors, you will need the adaptor.

    Best regards,

    Ming

  • Hi Ming,

    Thanks for your explanation. Those are what I was leant from the User Guide, schematics and BOM files.

    I will do more tests and get back to you later.

    Best regards,

    Lin

  • Hi Ming,

    The EVM board has been modified to support MSS_SPIB on J16. Now I'm modifying the sample code to support MSS_SPIB and our slave device.

    Here I have a question about code debugging and running.

    After building the project by right clicking on the project name and choosing Build Project, how will you do to debug or run the project code? By right clicking project name and choosing Debug As / 1 Code Composer Debug Session ? or some other way?

    Appreciate your sharing and advice.

    Best regards,

    Lin

  • Hi Ming,

    As we plan to connect AM273x with multiple devices via SPI, I want to use GPIO pins as CS for different device.  Questions are as below.

    - When I check the schematic of EVM board, the MSS_GPIO_2 is connected to LED D6. However, in the example.syscfg file the GPIO Pin(MSS_GPIO26). Do they match each other?  How should I choose the PAD numbers in the example.syscfg file?

    - Where can I find some other GPIO pin test points on the EVM board?

    Appreciate your help.

    Best regards,

    Lin

  • Hi Lin,

    In that case, you should use the MIBSPI in 3-pin mode (in example.syscfg)

    You should focus on the pins you will not use on J7 (60-pin connector). For example, the DBG_SPI_CS0 (MSS_SPIB_CS0 -> MSS_MIBSPIB_CS0 -> D19 mode 0 -> MSS_GPIO_4, according to Table 5-1 in AM273x datasheet). The D19 can be used for one of the CS pins.

    Another example is RCSS_SPIB_CS0 (RCSS_MIBSPIB_CS0 -> U17 mode 0 -> RCSS_GPIO_40 according to Table 5-1 in AM273x datasheet). The U17 can be used for one of the CS pins.

    Best regards,

    Ming

  • Hi Ming,

    Thanks for your reply and GPIO pin information. I checked the Table 5-1 of datasheet and confirmed the info. However, once I choose those pins D19 and U17, How/Where can I get them on the EVM board?

    Best regards,

    Lin

  • Hi Ming,

    Another question about MIBSPI setting in the example.syscfg file. What's the difference between Xbar Instance and SPI Instance? Should they be chosen the same value? now they are both the MSS_MIBSPIB / MSS_MIBSPIB or MSS_MIBSPIA / MSS_MIBSPIA.

    Thanks,

    Lin

  • Hi Lin,

    Yes, they should be the same.

    Best regards,

    Ming

  • Hi Lin,

    You will get them from the J7 using 60-pin breakout adapter (ZX100-QTH030-ST Samtec Breakout Adapter).

    Best regards,

    Ming

  • Thanks Ming, I will keep the setting.

    Regards,

    Lin

  • Thanks Ming,

    I will try to order the adapter and do more tests. Right now I'm working on 4 pin setting of MSS_SPIB connecting to J16. I will get back to you about the SPI testing and verifying.

    Best regards,

    Lin

  • Hi Ming,

    When I modify the mibspi_loopback.c file, I have following part of code:

    uint8_t const reg_addr = 0x1A;
    uint16_t const reg_data = 0xAA55;

    uint32_t lmx_frame = (0U << 23) | (reg_addr << 16) | reg_data; // 24-bit frame from LMX2595

    uint16_t txBuf[2];
    uint16_t rxBuf[2] = {0};

    txBuf[0] = (lmx_frame >> 8) & 0xFFFF; // Upper 16 bits
    txBuf[1] = (lmx_frame & 0xFF) << 8; // Lower 8 bits aligned to MSB

    When I build the project, got following error and warning messages:

    ../mibspi_loopback.c:71:1: warning: type specifier missing, defaults to 'int'; ISO C99 and later do not support implicit int [-Wimplicit-int]
    txBuf[0] = (lmx_frame >> 8) & 0xFFFF; // Upper 16 bits
    ^
    int
    ../mibspi_loopback.c:71:1: error: redefinition of 'txBuf' with a different type: 'int[0]' vs 'uint16_t[2]' (aka 'unsigned short[2]')
    ../mibspi_loopback.c:68:10: note: previous definition is here
    uint16_t txBuf[2];
    ^
    ../mibspi_loopback.c:72:1: warning: type specifier missing, defaults to 'int'; ISO C99 and later do not support implicit int [-Wimplicit-int]
    txBuf[1] = (lmx_frame & 0xFF) << 8; // Lower 8 bits aligned to MSB
    ^
    int
    ../mibspi_loopback.c:72:1: error: redefinition of 'txBuf' with a different type: 'int[1]' vs 'uint16_t[2]' (aka 'unsigned short[2]')
    ../mibspi_loopback.c:68:10: note: previous definition is here
    uint16_t txBuf[2];
    ^

    Do you have any hint and suggestion for those errors and warning? The screenshot is as below: (oh, sorry, seems I can't paste any screenshort here)

    expecting for your reply.

    Best regards,

    Lin

  • Hi Lin,

    One error is because of the type casting. lmx_frame is uint32_t and the txBuf[1] is uint16_t

    The other error is the txBuf has been defined twice (line 71 and line 68). One as the int and the other is uint16_t.

    Best regards,

    Ming 

  • Hi Ming,

    Any suggestion I can fix the error the txBuf has been defined twice (line 71 and line 68). One as the int and the other is uint16_t. I tried many ways to type cast and the other methods, but not succeed.

    As our connecting device needs 24-bit frame pattern, so I want to create the 2 16-bit data dynamically from the input register address and register data.

    uint16_t txBuf[2];

    txBuf[0] = (lmx_frame >> 8) & 0xFFFF;
    txBuf[1] = (lmx_frame & 0xFF) << 8;

    How can I avoid redefine the txBuf?

    Best regards,

    Lin

  • Hi Ming,

    BTW, if I hard code the txBuf as below

    uint16_t txBuf[2] = {0x1AAA, 0x5500};

    there will be no error. However, it's not flexible.

    Do need your help to fix those errors.

    Best regards,

    Lin

  • Hi Ming,

    FYI, once I put those parts of code into the void mibspi_loopback_main(void *args) () function, the errors and warning are gone. Now it passes the project build. I will focus on the debugging and testing.

    Best regards,

    Lin

  • Hi Lin,

    Try the following:

    txBuf[0] = (uint16_t)((lmx_frame >> 8) & 0xFFFF);
    txBuf[1] = (uint16_t)((lmx_frame & 0xFF) << 8);

    Best regards,

    Ming

  • Thanks Ming,

    I get same error messages, if I put the part of code outside of the function. However, As I said in previous message, if I move those parts of code into the function, it works well. Now my code is as below FYI.

    #include <kernel/dpl/DebugP.h>
    #include <kernel/dpl/SemaphoreP.h>
    #include <kernel/dpl/HwiP.h>
    #include <kernel/dpl/ClockP.h>
    #include <drivers/mibspi.h>
    #include "ti_drivers_config.h"
    #include "ti_drivers_open_close.h"
    #include "ti_board_open_close.h"
    /*
    uint32_t lmx_frame = 0x1AAA55;
    uint16_t txBuf[2] = {0x1AAA, 0x5500};
    uint16_t rxBuf[2] = { 0 };
    */
    /*
    uint8_t const reg_addr = 0x1A; /// uint8_t const, no need
    uint16_t const reg_data = 0xAA55; /// uint16_t const, no need

    uint32_t lmx_frame = (0U << 23) | (reg_addr << 16) | reg_data; // 24-bit frame from LMX2595

    uint16_t txBuf[2] = {0};
    uint16_t rxBuf[2] = {0};

    txBuf[0] = (uint16_t)(lmx_frame >> 8) & 0xFFFF; // Upper 16 bits
    txBuf[1] = (uint16_t)(lmx_frame & 0xFF) << 8; // Lower 8 bits aligned to MSB
    */

    void mibspi_loopback_main(void *args)
    {
    int32_t transferOK;
    MIBSPI_Transaction spiTransaction;


    uint8_t reg_addr = 0x1A; /// uint8_t const, no need
    uint16_t reg_data = 0xAA55; /// uint16_t const, no need

    uint32_t lmx_frame = (0U << 23) | (reg_addr << 16) | reg_data; // 24-bit frame from LMX2595

    uint16_t txBuf[2] = {0};
    uint16_t rxBuf[2] = {0};

    txBuf[0] = (lmx_frame >> 8) & 0xFFFF; // Upper 16 bits
    txBuf[1] = (lmx_frame & 0xFF) << 8; // Lower 8 bits aligned to MSB


    Drivers_open();
    Board_driversOpen();

    DebugP_log("[MIBSPI] MSS_SPIB_J16 started ...\r\n");

    /* Initiate transfer */
    spiTransaction.count = 2; /// 2 16-bit data for 24-bit frame
    spiTransaction.txBuf = (void *)txBuf;
    spiTransaction.rxBuf = (void *)rxBuf;
    spiTransaction.peripheralIndex = 0U;
    spiTransaction.arg = NULL;

    /// check the handle is created well
    DebugP_log("SPIB Handle Address: 0x%x\r\n", gMibspiHandle[MSS_SPIB_J16]);

    /// start SPI transfer
    transferOK = MIBSPI_transfer(gMibspiHandle[MSS_SPIB_J16], &spiTransaction);

    /// check the transfer results
    DebugP_log("transferOK = %d, spiTransaction.status = %d\r\n", transferOK, spiTransaction.status);

    if((SystemP_SUCCESS != transferOK) ||
    (MIBSPI_TRANSFER_COMPLETED != spiTransaction.status))
    {
    DebugP_log("SPI transfer failed!\r\n");
    DebugP_assert(FALSE); /* MIBSPI transfer failed!! */
    }
    else
    {
    DebugP_log("SPI transfer succeeded!\r\n");
    }

    Board_driversClose();
    Drivers_close();

    return;
    }

    Before checking and verifying SPI signals on J16 header, I have some questions.

    My MIBSPI settings in exampl.syscfg file are as below:

    example.syscfg / TI DRIVERS (20) / MIBSPI 2/4

    Name MSS_SPIB_J16
    Mode of Operation Controller
    Clock Frequency (Hz) 5000000
    Transmit End Delay 0x0
    Chip Select Active Delay 0x0
    Delay Between Transmissions 0x0
    Data Size 16
    Frame Format Mode 0 (POL0 PHA0)
    Transfer Mode Blocking
    Enable Multi ICount Support unchecked
    Transfer Timeout 0xFFFFFFFF
    Pin Mode 4 Pin Mode with CS
    Shift Format MSB shift out first
    Enable DMA unchecked
    Number of Transfer Groups 1
    Show Advanced Config unchecked
    XBar Instance MSS_MIBSPIB
    SPI Instance MSS_MIBSPIB
    Signals Pins Up/Down
    MIBSPI CLK Pin(MSS_MIBSPIB_CLK) PAD_CV/V19 Pull Up
    MIBSPI MISO Pin(MSS_MIBSPIB_MISO) PAD_CU/V18 Pull Up
    MIBSPI MOSI Pin(MSS_MIBSPIB_MOSI) PAD_CT/U19 Pull Up
    MIBSPI Channel Configuration
    MIBSPI Channel Configuration 0
    Peripheral Chip-select 0
    DMA Request Line 0
    Signals Pins
    CS Pin PAD_CX/W18 No Pull

    For the 4 SPI signals, there are some other PAD choices available. Which one will be the correct one for connecting to J16 header pin? Or any of them are correct?

    For my above settings and code, how can I verify the SPI signals on J16 of EVM?

    Detailed instructions are appreciated.

    Best regards,

    Lin

  • Hi Ming,

    One more question. Which pin or TP can I use as a ground when I measure J16 pin signals with scope?

    Thanks,

    Lin

  • Hi Lin,

    J24 pin 3, 11, 21, 29, 8, 16 and 26 are GND.

    Best regards,

    Ming

  • Thanks Ming, Got it.

    Could you verify my 4 pin's PAD choices?

    Best regards,

    Lin

  • Hi Lin,

    As long as they are not used and you can access to them on the AM273 EVM or via breakout adaptor, then they are OK. Plus you can change them easily.

    Best regards,

    Ming

  • Hi Ming,

    FYI, I have done the testing SPI signals on J16 of EVM. 

    Only one set of pad mapping is working as below:

    MIBSPI CLK Pin(MSS_MIBSPIB_CLK) PAD_AJ/D18
    MIBSPI MISO Pin(MSS_MIBSPIB_MISO) PAD_AI/C19
    MIBSPI MOSI Pin(MSS_MIBSPIB_MOSI) PAD_AH/C18
    CS Pin PAD_AA/E18

    CS Signal on the R5 pin of J16 is very, not a clean lower level square signal. Only can capture one group of signal and MOSI data only match with upper 16-bit data. Can't display the lower 16-bit data on the scope.

    Do you have any comments or explanation on the above results?

    Best regards,

    Lin

  • Hi Lin,

    There two things you may need to pay attention to:

    1. The CS0 should be D19, F2 or U17. The E18 is for CS1. If you do want to use CS1, then the "Peripheral Chip-select" has to be set to 1 not 0 (default)

    2. The Saleae capture voltage (1.8V/3.3V) has to match the ones used for MIBSPI (1.8V/3.3V) 

    Best regards,

    Ming

  • Hi Ming,

    Thank you very much for your information.

    Yes, by try errors I find D19 is good choice for CS0. However, is there a better way to find it such as by reading and tracing on schematics or the other design documents? Or how did you know D19, F2 and U17 are good ones?

    I will pay attention to the signal levels.

    Best regards,

    Lin

  • Hi Lin,

    Please refer to AM273x datasheet table 5-36, 5-37, 5-38 and 5-39 for details.

    Best regards,

    Ming

  • Hi Ming,

    So Far the MSS_SPIB 4 pin mode is working well and I have verified by checking the signal with scope. Thank you very much for your help and support.

    Now I want to focus on MSS_SPIB 3 pin mode + GPIO pins as CS function.

    Could you give more detailed instruction on one example pin as: DBG_SPI_CS0 (MSS_SPIB_CS0 -> MSS_MIBSPIB_CS0 -> D19 mode 0 -> MSS_GPIO_4, according to Table 5-1 in AM273x datasheet).? When I check datasheet Table 5-1, I am still not confident what I should do.

    Appreciate your help and time.

    Best regards,

    Lin

  • Hi Lin,

    According to AM273x datasheet, the D19 can be used either as MSS_MIBSPIB_CS0 (mode 1) or MSS_GPIO_4 (mode 0). When you use the SPI 4 pin mode, the syscfg will configure the DBG_SPI_CS0 (D19) to be mode 1. When you use the SPI 3 pin mode, the syscfg will not configure the DBG_SPI_CS0 (D19) at all. It is up to you to configure it in the syscfg under the GPIO (the D19 has to be configure as the GPIO pin output, mode 0 etc). You are also responsible to set the D19 to high when the SPI is ready to transmit/receive data in your software.

    For how to configure and use the GPIO pins, please refer to the GPIO example in MCU+ SDK:  C:\ti\mcu_plus_sdk_am273x_09_02_00_60\examples\drivers\gpio\gpio_led_blink

    Best regards,

    Ming

  • Hi Ming,

    Thank you for your detailed instruction and explanation. I will try to set it and test it. I will update you my status.

    Best regards,

    Lin

  • Hi Ming,

    Here is my latest status.

    I made following modifications:
    1) .syscfg
    A) Pin Mode 3 Pin Mode
    B) unchecked CS Hold Enable under Advanced Config
    C) unchecked Show Advanced Config
    D) add GPIO setting
    Name GPIO_LMX_CS
    PIN Direction Output
    Trigger Type None
    Trigger Level Low
    Open Drain Disable
    XBar Instance MSS_GPIO
    GPIO Peripheral MSS_GPIO0
    Signals Pins Pull Up/Down
    GPIO Pin(MSS_GPIO4) PAD_AK/D19 No Pull
    2) mibspi_loopback.c
    A) #include <drivers/gpio.h>
    B) uint32_t gpioBaseAddr, pinNum;
    C) /* Get address after translation translate */
    gpioBaseAddr = (uint32_t) AddrTranslateP_getLocalAddr(GPIO_LMX_CS_BASE_ADDR);
    pinNum = GPIO_LMX_CS_PIN;
    GPIO_setDirMode(gpioBaseAddr, pinNum, GPIO_LMX_CS_DIR);
    D) GPIO_pinWriteLow(gpioBaseAddr, pinNum); // Assert CS (Active Low)
    transferOK = MIBSPI_transfer(gMibspiHandle[MSS_SPIB_J16], &spiTransaction);
    GPIO_pinWriteHigh(gpioBaseAddr, pinNum); // Deassert CS

    After build and run my latest code, I can get SPI CLK and SPI MOSI signals from the pins of J16 on the EVM, but I can NOT get the GPIO CS signal from the pin 7 of J7 on the EVM. However, I CAN get the GPIO CS signal on the CS0 pin of the J16.

    The S2 was set to PMIC_SPI position as before, not changed.

    If I change S2 to DBG_SPI position, no CLK and MOSI on J16, and still NO GPIO CS signal on the pin 7 of J7.

    Are all my above results correct? Did I miss anything to get the GPIO CS signal from the pin7 of J7?

    Could you help me to check it? Or could you share your correct setting?

    Best regards,

    Lin

  • Hi Lin,

    The test result matches your settings. The J16 is for PMIC_SPI signals, so the S2 should be on the PMIC SPI. The D19 mode 0 is the MSS_GPIO_4 --> PMIC_SPI_CS0. 

    However, when you switch S2 to DBG_SPI, pin 7 of J7 DBG_SPI_CS0 should have been connected to the MSS_SPIB_CS0 --> MSS_MIBSPIB_CS0 --> D19, so you should have seen it pulled low when the CS is enabled.

    Best regards,

    Ming.

  • Hi Ming,

    S2 to PMIC_SPI, the results are reasonable. However, when S2 to DBG_SPI, I checked pin7 of J7 very carefully, it has no 3.3V signal toggle. GPIO part of code is same not change. Could you or any other member verify it on your side?

    Best regards,

    Lin

  • Hi Lin,

    With S2 on DBG_SPI, I did my testing with gpio_led_blink_am273x-evm_r5fss0-0_nortos_ti-arm-clang. The only change I made is to change the MSS_GPIO26(H2) to MSS_GPIO4 (D19):

    Here is what I get from the pin7 of J7: 

    It is expected result.

    Best regards,

    Ming

  • Hi Ming,

    Thank you so much for you sharing the results with me. Although I can't get the same results as yours on my EVM, I will assume that it working for me.

    When we design our prototype we will pay attention to that.

    Two more questions for you before we close this case. Where are you physically located? Is it possible for you to provide in person support either you come to our office in Huntington Beach, CA US or I can go to your office with my boards?

    Best regards,

    Lin

  • Hi Lin,

    Are you using the ZX100-QTH030-ST Samtec Breakout Adapter on J7 to get the pin7 and Saleae Logic Pro to capture the signals?

    Have you connected the pin8 of J7 for GND?

    Best regards,

    Ming

  • Hi Ming, 

    Thank you very much for your follow up questions. 

    I have ordered the  ZX100-QTH030-ST Samtec Breakout Adapter for my test, it will arrive my office next Monday. I just asked our technician to solder a test wire from pin 7 of the J7. And I used RIGOL MSO5104 scope to capture the signal not Saleae Logic Pro.

    No, I still use pin 29 and 26 of J24 as GND not pin8 of J7. Do I have to use the pin 8 as GND to capture the signal on pin 7 of J7?

    Best regards,

    Lin

     

  • Hi Lin,

    That is potentially the problem is. I used the ZX100-QTH030-ST Samtec Breakout Adapter, so I am sure I measure the correct pin7 of J7.

    No, the GND on J24 works too.

    You can repeat your test once the breakout adaptor arrived. I bet it will work.

    Best regards,

    Ming