Part Number: AM263P4-Q1
Other Parts Discussed in Thread: AM263P4
Tool/software:
The AM263P4 part requires 3.3 volts and 1.2 volts as inputs. It then makes 1.8 volts from internal Low drop out (LDO) regulators. Which of these power supplies ( if any) need to be up to its valid operating level before I apply a voltage on an A/D input? Note this part has 5 A/Ds with 6 inputs a piece and also 2 shared calibration inputs that are routed to each A/D.
Thank you
Whitney Ballard
Whitney.ballard@collins.com