Part Number: MSPM0L2227
Tool/software:
Hi All,
I have a question about how to use EEPROM sample code.
The customer is currently using Renesas RL78, so Data Flash is available.
The question is whether background operations are possible when implementing data storage using M0 EEPROM Emulation software.
Is it possible to store arbitrary variables using EEPROM emulation without stopping the main control?
Additionally, it states that Type A can store 64 bytes, 128 bytes, or 256 bytes,
and Type B can store 16-bit or 32-bit data.
The customer wishes to store data of 16-byte or 32-byte sizes. Is it possible to freely change the data size? If not, please advise on a method to store data of 16-byte or 32-byte sizes.
Additionally, the RL78 uses 2 kB of Data Flash.
Furthermore, the header size is reportedly large.
Please specify the maximum capacity of Data Flash that can be handled by the MSPM0L2227.
Best Regards,
Ito