Part Number: AM2612
Tool/software:
Hi, experts,
In AM2612 datasheet, it is mentioned "If the internal temp diode is being used this pin must be connected to the 1.2V/1.25V power rail. If the internal temp diode is not being used this pin can be connected (shorted) directly to ground (VSS)."

In AM2612 TRM, it is mentioned "The TM module on the device enables thermal management of the device by providing control of on-chip temperature sensors."
Customer wants to confirm whether the "" and "" are the same or different components. If VDD_TEMP is connected directly to ground, can TSENSE0 and TSENSE1 work normally?

Thanks.