Part Number: MSPM0C1104
Other Parts Discussed in Thread: SYSCONFIG, MSPM0C1103
Tool/software:
Hi I'm working on a 8 pin version using one i/o PIN 6, one uart pins 1 & 8 and a PWM pin 7 but no longer able to see an output on pin 7 .
the same C source works with different pins on LP-MSPM0C1104.
Debuf is (of course) disabled to use 6 & 7 but probably I miss some setup in sysconfig. due to the fact I cannot recover programmed parts (flasher cannot work on already programmed parts)
I kindly ask you a help.
thanks !
p.s. is there a way to recover already programmed parts?
-----
/**
* These arguments were used when this file was generated. They will be automatically applied on subsequent loads
* via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
* @cliArgs --device "MSPM0C110X" --part "Default" --package "SOT-8(DDF)" --product "mspm0_sdk@2.04.00.06"
* @v2CliArgs --device "MSPM0C1103" --package "SOT-8(DDF)" --product "mspm0_sdk@2.04.00.06"
* @versions {"tool":"1.23.0+4000"}
*/
/**
* Import the modules used in this configuration.
*/
const Board = scripting.addModule("/ti/driverlib/Board");
const GPIO = scripting.addModule("/ti/driverlib/GPIO", {}, false);
const GPIO1 = GPIO.addInstance();
const PWM = scripting.addModule("/ti/driverlib/PWM", {}, false);
const PWM1 = PWM.addInstance();
const SYSCTL = scripting.addModule("/ti/driverlib/SYSCTL");
const UART = scripting.addModule("/ti/driverlib/UART", {}, false);
const UART1 = UART.addInstance();
/**
* Write custom configuration values to the imported modules.
*/
Board.debugOn = false;
scripting.suppress("Debug Disabled! Code Cannot be Debugged", Board, "debugOn");
GPIO1.$name = "Sensore";
GPIO1.port = "PORTA";
GPIO1.associatedPins[0].$name = "PIN_sensore";
GPIO1.associatedPins[0].pin.$assign = "PA19";
PWM1.$name = "PWM_0";
PWM1.ccIndex = [0];
PWM1.timerStartTimer = true;
PWM1.clockDivider = 2;
PWM1.PWM_CHANNEL_0.$name = "ti_driverlib_pwm_PWMTimerCC0";
PWM1.PWM_CHANNEL_0.dutyCycle = 25;
PWM1.PWM_CHANNEL_0.invert = true;
PWM1.ccp0PinConfig.$name = "ti_driverlib_gpio_GPIOPinGeneric2";
PWM1.peripheral.$assign = "TIMA0";
PWM1.peripheral.ccp0Pin.$assign = "PA20";
SYSCTL.peripheral.$assign = "SYSCTL";
UART1.$name = "UART_0";
UART1.uartClkSrc = "LFCLK";
UART1.ovsRate = "3";
UART1.rxFifoThreshold = "DL_UART_RX_FIFO_LEVEL_ONE_ENTRY";
UART1.enabledInterrupts = ["RX"];
UART1.peripheral.$assign = "UART0";
UART1.peripheral.rxPin.$assign = "PA24";
UART1.peripheral.txPin.$assign = "PA27";
UART1.txPinConfig.$name = "ti_driverlib_gpio_GPIOPinGeneric0";
UART1.txPinConfig.enableConfig = true;
UART1.txPinConfig.internalResistor = "PULL_UP";
UART1.rxPinConfig.$name = "ti_driverlib_gpio_GPIOPinGeneric1";
UART1.rxPinConfig.enableConfig = true;
UART1.rxPinConfig.internalResistor = "PULL_UP";
const ProjectConfig = scripting.addModule("/ti/project_config/ProjectConfig", {}, false);
ProjectConfig.migrationCondition = true;
/**
* Pinmux solution for unlocked pins/peripherals. This ensures that minor changes to the automatic solver in a future
* version of the tool will not impact the pinmux you originally saw. These lines can be completely deleted in order to
* re-solve from scratch.
*/
Board.peripheral.$suggestSolution = "DEBUGSS";