Part Number: MSPM0L1305
Tool/software:
Im having issues with some GPIO output pins. Two of the output pins aren't going high when using DL_GPIO_setPins() specifically FET_EN and DRV_EN_UVLO. I used a barebone "hello world" program to try to toggle the pins and used a meter to test the voltage on the pins to verify. Both pins read 0 volts. Not sure if I'm missing a configuration setting for the pins or if this is a HW issue. Attached are the config files and main file for the dummy test as well as the main.main.zipdummy_test.zip