This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEMU110-U: customer report issue trying to use emulator to program the device flash

Part Number: TMDSEMU110-U

Tool/software:

Hi Expert

Customer uses F28P55 in their new design, they use our TMDSEMU110-U as emulator to program the device flash, but see the issue reported sometimes, could you please help to check in what condition, customer will see this issue and how to fix it?

there is another issue reported by customer, only restarting the computer can resolve the issue:

Thanks

Joe

  • Hello,

    but see the issue reported sometimes

    Sounds like this is a sporadic issue that happens only occasionally?

    As for the first issue (-1156), it means he device is in low power run mode. Depending on the severity of the condition, the JTAG debugger may or may not be able to bring it out of this mode. What happens when "Yes" is pressed?

    As for the second issue, The error below typically happens if the debugger is not detecting power. If the PC needs to be restarted to resolve it, then that would indicate that it is not specifically a hardware issue. Is this also a occasional issue?

    Thanks

    ki

  • Hi Ki

    What happens when "Yes" is pressed?

    After clicking yes, the GUI will stuck here for a long time (half hour).

    As for the second issue

    it is an occasional issue, but happens many times with different PCs in customer side.

    thanks

    Joe

  • These types of occasional issues are difficult to debug. It means there is not anything inherently wrong but instead it is some stability issue. Have these issues ever been seen with the CCS IDE? How often does the first issue occur?

  • Hi Ki

    I let them to ship back some emulators before and I saw the 5V input capacitor is short circuit and 5V to 3.3V DCDC is broken. So I doubt that might be the USB power supply is not stable with customer computer, and suggest then to use the isolated power supply like ISO-USB to power up the emulator, but they didn't take my suggestion. Now seems the same issue happens. I will push them to debug the PC HW but not our emulators.

    I will close this thread. thanks for your support.

    Best regards

    Joe

  • Ok, thank you for the update!

  • Hi Ki

    I debug in customer today, I find the Pin5 is 3.3V when I measure the voltage of XDS110 input pin

    But when I use test connection function with ccs the below issue is still reported by ccs:

    I do not have the TMDSEMU110-U schematic, so I cannot measure the TM4C MCU pins to see whether the MCU input is correct.

    But I checked the F28P55 power supply is LM63635 and schematic looks find.

    Could you please share the XDS110 Pin5 related schematic so that I can bug further?

    Thanks

    joe

  • Part Number: TMDSEMU110-U

    Tool/software:

    Hi Expert 

    It is the continue question of this E2E thread: link

    I debugged the emulator in customer, I found the Pin5 is 3.3V when I measure the voltage of XDS110 input pin

    But when I used test connection function with ccs the below issue was still reported by ccs:

    I did not have the TMDSEMU110-U schematic, so I could not measure the TM4C MCU pins to see whether the MCU input was correct.

    But I checked the F28P55 power supply is LM63635 and schematic looks find.

    Could you please share the XDS110 Pin5 related schematic so that I can bug further?

    Thanks

    joe

  • Hello,

    Please allow me another day to retrieve the requested schematic. 

    Is this issue isolated to one debugger, or has this happened on multiple probes?

    Best,

    Matt

  • Hi Matt

    Thanks for your support, this issue happened in multiple debug probes, including onboard XDS110 of MSPM0, onboard XDS110 of F28P55 (total 8 pcs), but first happen in TMDSEMU110-U since customer only has one TMDSEMU110-U for now.

    Best regards

    Joe

  • Hello,

    I'll will share the schematic with you offline. 

    I let them to ship back some emulators before and I saw the 5V input capacitor is short circuit and 5V to 3.3V DCDC is broken. So I doubt that might be the USB power supply is not stable with customer computer, and suggest then to use the isolated power supply like ISO-USB to power up the emulator, but they didn't take my suggestion.

    Has the customer tried this? Since the issue has been repeated across different probes, it may be worth evaluating this option.

    Best,

    Matt

  • Hi Matt 

    We did this but they did not feedback to me whether the PC USB port has any issue, but for now TMDSEMU110-U issue is that the emulator cannot detect the Pin5 3.3V signal which is the PCBA power, so it is not the issue of PC USB connection.

    I shared the schematic to customer HW RD will see what issue happened on this probe.

    Thanks

    Joe

  • Hi Joe,

    That's interesting, please keep this thread updated of any progression. Can you share the customer's target configuration file ccxml with me? 

    Best,

    Matt

  • Hi Joe,

    Can you also please ask the customer when they purchased the XDS110 and the serial number?

    Best,

    Matt

  • Hi Matt

    Will do that today.

  • Hi Joe,

    Thank you for checking for me, we're investigating if this could be a widespread issue.

    Best,

    Matt

  • Hi Matt

    The Serial # 8252002054, but RD cannot get the accurate purchasing time, it should be in JUN/ JUL.

    Thanks

    Joe 

  • Hi Joe,

    Thank you for the additional details, that helps a lot.

    Can you also share the customer's ccxml file with me?

    Best,

    Matt

  • Hi Matt

    Please see the ccxml file attached:https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/908/TMS320F28P559SJ9_2D00_Q1.ccxml

    Thanks

    Joe

  • Hi Joe,

    Thank you, I will take a look into this and test on my local setup.

    Best,

    Matt

  • Hi Matt 

    Do you have the plan on this? When can I expect the next discussion.

    Thanks

    Joe

  • Hello,

    I was able to use the customer's target config without issues. My colleague is OoO this week and will discuss the issue further once they return.

    Best,

    Matt

  • Hello,

    To update this thread: it has been found the PC was not providing a stable ground, causing damage to the XDS110. Internal debugging is underway to repair the debugger. 

    I will close the thread now.

    Best,

    Matt