Part Number: MSPM0G1107
Tool/software:
Hi Team,
Our customer have
tried the example bsl_host_mcu_to_mspm0g1x0x_g3x0x_target_uart, it can success to update FW.
But there are few questions need comments.
- How to config the App1 structure which defined in application_image_uart.h. What are the purposes of these two partitions(1400, 16)?

- How can I merge the code to our application code? I'm still a bit puzzled about how to set the BSL UART baud rate from 9600 to 115200 with the BSL Plugin sample code?
- How to avoid to erase the user data partition “EEPROM” when we do the OTA update by SBL UART?
MEMORY
{
FLASH (RX) : origin = 0x00000000, length = 0x0001F000
EEPROM (RWX) : origin = 0x0001F000, length = 0x00001000
SRAM (RWX) : origin = 0x20200000, length = 0x00008000
BCR_CONFIG (R) : origin = 0x41C00000, length = 0x00000080
BSL_CONFIG (R) : origin = 0x41C00100, length = 0x00000080
}
Thanks for your support in advance!