Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:

On MSPM0G3507, the four-channel ADC uses DMA mode, with uint16_t ADC_VALUE[100][4]; 50us*4*100=20ms. Theoretically, one ADC DMA should be completed within 20ms. However, in actual measurements, it takes more than 100ms to complete one DMA. What could be the possible reasons for this? In the sysconfig, the Transfer Mode of the DMA Channel has been configured as Repeat Single to prevent program interference.