Part Number: AM2634
Tool/software:
Hi Team
I have a query regarding the CPSW Ethernet configuration. I have set up the CPSW interface in RGMII mode and configured it for 1Gbps operation. However, I am unable to achieve communication at this speed — specifically, I am not able to ping the device when 1Gbps is configured.
On the other hand, when I set the PHY speed to Auto, 10Mbps, or 100Mbps, the ping works successfully and I am able to communicate over the network at the corresponding speed.
Given this behavior, I would like to understand the following:
-
Is there any specific configuration or hardware setting required to enable and successfully operate at 1Gbps using RGMII with CPSW?
-
Does the AM263x CPSW interface fully support 1Gbps operation in RGMII mode, or is it limited to 10/100Mbps?
-
Are there any timing adjustments (e.g., RGMII TX/RX delay, internal/external delay) or board-level constraints I should verify?
I would appreciate any guidance or documentation references that could help me ensure correct 1Gbps operation.