This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: Power supply for high level functional safety

Genius 3186 points

Part Number: AM2434
Other Parts Discussed in Thread: LP8733, TPS65219

Tool/software:

Hello,

We are considering AM243x for high level functional safety machine.

Could you check these questions?

We want to compliant for SIL3, categoly 4 (ISO 13849)

Question 1

For these function safety compliant, we believe use LP87334DRHDR.

Do you have another option of PMIC?

Question 2

I believe it require Lockstep hardware for compliant.

Is it enough below hardwere for voltage monitoring ? (Is it need another voltage monitoring port for diagnostics)

source-------LP8733(PMIC1)-----AM243x(CPU1)

                                                       | (communication for diagnostics)

source-------LP8733(PMIC2)-----AM243x(CPU2)

Best Regards,

GR

  • Hi experts,

    Do you have update?

    Thanks,

    GR

  • Hi GR,

    Apologies for the delay, it took some time for your question to be routed to the correct team. 

    For power solutions for AM243x, LP8733 or TPS65219 are the recommended PMICs:

    However, these PMICs are general purpose and not Functional-Safety compliant devices themselves. 
    So yes, they will need external voltage monitors for the system to be considered functional safety compliant. 

    I am not sure if I am understanding your hardware outline correctly, where are you proposing the voltage monitor should be connected?

    We do have FIT rate and FMD documentation available for the TPS65219-Q1 (automotive rated TPS65219) to assist with safety assessment here. 
    But this device was not specifically designed according to ISO26262 standards.

    For a complete functional safety-compliant PMIC solution, then TPS6594-Q1 would be the recommended device.
    (Functional safety documentation is available upon request, only under NDA) 

    Best Regards, 
    Sarah

  • Hi Sarah,

    Thanks for your information.

    I will contact local sales team for access the document.

    Best Regards,

    GR