This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3519: About ROM based BSL and Flash based Secondary BSL

Part Number: MSPM0G3519

Tool/software:

Hi team,

My customer have some questions about about ROM based BSL and Flash based Secondary BSL,

  1. If we use Software Invoke, only two pins are needed for I2C interface, correct?
  2. For ROM based BSL solution, can we re-configure I2C slave address? What is the default address?
  3. For ROM based BSL with Plug-in interface solution, can we re-configure I2C slave address?
  4. Do you have any data about time for erase/programming 512kB based on ROM based BSL solution?
  5. If we select Flash Based Secondary BSL, do we need to disable ROM based BSL because we use the same I2C interface?