Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN, , PCF8574A
Tool/software:
Hello,
I am using TMS570LS3137 board as I2C master device, and I am using PCF8574T as I2C slave. I initialized the I2C peripheral in HalCoGen and pinmuxed the SDA and SCL pins in pin-mux. My purpose is to write some mesages on the LCD. But when I try to initialize the lcd with lcd_init_AUEHSIM(&lcd); , it never goes out of
while ((i2c->STR & (uint32)I2C_TX_INT) == 0U)
{
} /* Wait */
function which is in i2cSend() function which is in i2c.c file. I will provide all the necessary codes with explanations in blue comments which are i2c.c, sys_main.c, i2c_lcd.c. Additionaly, I am providing the source files.
/** @file i2c.c
* @brief I2C Driver Implementation File
* @date 11-Dec-2018
* @version 04.07.01
*
*/
/*
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
#include "i2c.h"
#include "sys_vim.h"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/** @struct g_i2CTransfer
* @brief Interrupt mode globals
*
*/
static struct g_i2cTransfer
{
uint32 mode;
uint32 length;
uint8 * data;
} g_i2cTransfer_t;
/* USER CODE BEGIN (2) */
/* USER CODE END */
/** @fn void i2cInit(void)
* @brief Initializes the i2c Driver
*
* This function initializes the i2c module.
*/
/* SourceId : I2C_SourceId_001 */
/* DesignId : I2C_DesignId_001 */
/* Requirements : HL_SR279 */
void i2cInit(void)
{
/* USER CODE BEGIN (3) */
/* USER CODE END */
/** @b initialize @b I2C */
/** - i2c Enter reset */
i2cREG1->MDR = (uint32)((uint32)0U << 5U);
/** - set i2c mode */
i2cREG1->MDR = (uint32)((uint32)0U << 15U) /* nack mode */
| (uint32)((uint32)0U << 14U) /* free running */
| (uint32)(0U) /* start condition - master only */
| (uint32)((uint32)1U <<11U) /* stop condition */
| (uint32)((uint32)1U <<10U) /* Master/Slave mode */
| (uint32)((uint32)I2C_TRANSMITTER) /* Transmitter/receiver */
| (uint32)((uint32)I2C_7BIT_AMODE) /* xpanded address */
| (uint32)((uint32)0U << 7U) /* repeat mode */
| (uint32)((uint32)0U << 6U) /* digital loop back */
| (uint32)((uint32)0U << 4U) /* start byte - master only */
| (uint32)((uint32)0U << 3U) /* free data format */
| (uint32)(I2C_8_BIT); /* bit count */
/** - set i2c Backward Compatibility mode */
i2cREG1->EMDR = 0U;
/** - Disable DMA */
i2cREG1->DMACR = 0x00U;
/** - set i2c data count */
i2cREG1->CNT = 8U;
/** - disable all interrupts */
i2cREG1->IMR = 0x00U;
/** - set prescale */
i2cREG1->PSC = 10U;
/** - set clock rate */
i2cREG1->CKH = 36U;
i2cREG1->CKL = 36U;
/** - set i2c pins functional mode */
i2cREG1->PFNC = (0U);
/** - set i2c pins default output value */
i2cREG1->DOUT = (uint32)((uint32)1U << 1U) /* sda pin */
| (uint32)(1U); /* scl pin */
/** - set i2c pins output direction */
i2cREG1->DIR = (uint32)((uint32)0U << 1U) /* sda pin */
| (uint32)(0U); /* scl pin */
/** - set i2c pins open drain enable */
i2cREG1->PDR = (uint32)((uint32)0U << 1U) /* sda pin */
| (uint32)(0U); /* scl pin */
/** - set i2c pins pullup/pulldown enable */
i2cREG1->PDIS = (uint32)((uint32)0U << 1U) /* sda pin */
| (uint32)(0U); /* scl pin */
/** - set i2c pins pullup/pulldown select */
i2cREG1->PSEL = (uint32)((uint32)1U << 1U) /* sda pin */
| (uint32)(1U); /* scl pin */
/** - set interrupt enable */
i2cREG1->IMR = (uint32)((uint32)0U << 6U) /* Address as slave interrupt */
| (uint32)((uint32)0U << 5U) /* Stop Condition detect interrupt */
| (uint32)((uint32)0U << 4U) /* Transmit data ready interrupt */
| (uint32)((uint32)0U << 3U) /* Receive data ready interrupt */
| (uint32)((uint32)0U << 2U) /* Register Access ready interrupt */
| (uint32)((uint32)0U << 1U) /* No Acknowledgement interrupt */
| (uint32)((uint32)0U); /* Arbitration Lost interrupt */
/** - i2c Out of reset */
i2cREG1->MDR |= (uint32)I2C_RESET_OUT;
/** - initialize global transfer variables */
g_i2cTransfer_t.mode = (uint32)0U << 4U;
g_i2cTransfer_t.length = 0U;
/* USER CODE BEGIN (4) */
/* USER CODE END */
}
/** @fn void i2cSetOwnAdd(i2cBASE_t *i2c, uint32 oadd)
* @brief Set I2C Own Address
* @param[in] oadd - I2C Own address (7-bit or 10 -bit address)
* @param[in] i2c - i2c module base address
* Set the Own address of the I2C module.
*/
/* SourceId : I2C_SourceId_002 */
/* DesignId : I2C_DesignId_002 */
/* Requirements : HL_SR280 */
void i2cSetOwnAdd(i2cBASE_t *i2c, uint32 oadd)
{
i2c->OAR = oadd; /* set own address */
}
/** @fn void i2cSetSlaveAdd(i2cBASE_t *i2c, uint32 sadd)
* @brief Set Port Direction
* @param[in] sadd - I2C Slave address
* @param[in] i2c - i2c module base address
* Set the Slave address to communicate which is must in Master mode.
*/
/* SourceId : I2C_SourceId_003 */
/* DesignId : I2C_DesignId_003 */
/* Requirements : HL_SR281 */
void i2cSetSlaveAdd(i2cBASE_t *i2c, uint32 sadd)
{
i2c->SAR = sadd; /* set slave address */
}
/** @fn void i2cSetBaudrate(i2cBASE_t *i2c, uint32 baud)
* @brief Change baudrate at runtime.
* @param[in] i2c - i2c module base address
* @param[in] baud - baudrate in KHz
*
* Change the i2c baudrate at runtime. The I2C module needs to be taken to reset( nIRS=0 in I2CMDR) in order to change baud rate.
*/
/* SourceId : I2C_SourceId_004 */
/* DesignId : I2C_DesignId_004 */
/* Requirements : HL_SR282 */
void i2cSetBaudrate(i2cBASE_t *i2c, uint32 baud)
{
uint32 prescale;
uint32 d;
uint32 ck;
float64 vclk = 90.000F * 1000000.0F;
float64 divider= 0.0F;
uint32 temp = 0U;
/* USER CODE BEGIN (5) */
/* USER CODE END */
divider = vclk / 8000000.0F;
prescale = (uint32)divider - 1U;
if(prescale>=2U)
{
d = 5U;
}
else
{
d = (prescale != 0U) ? 6U : 7U;
}
temp = 2U * baud * 1000U * (prescale + 1U);
divider = vclk / ((float64)temp);
ck = (uint32)divider - d;
i2c->PSC = prescale;
i2c->CKH = ck;
i2c->CKL = ck;
/* USER CODE BEGIN (6) */
/* USER CODE END */
}
/** @fn void i2cSetStart(i2cBASE_t *i2c)
* @brief Set i2c start condition
* @param[in] i2c - i2c module base address
* Set i2c to generate a start bit (Only in Master mode)
*/
/* SourceId : I2C_SourceId_005 */
/* DesignId : I2C_DesignId_015 */
/* Requirements : HL_SR293 */
void i2cSetStart(i2cBASE_t *i2c)
{
/* USER CODE BEGIN (7) */
/* USER CODE END */
i2c->MDR |= (uint32)I2C_START_COND; /* set start condition */
/* USER CODE BEGIN (8) */
/* USER CODE END */
}
/** @fn void i2cSetStop(i2cBASE_t *i2c)
* @brief Set i2c stop condition
* @param[in] i2c - i2c module base address
* Set i2c to generate a stop bit (Only in Master mode)
*/
/* SourceId : I2C_SourceId_006 */
/* DesignId : I2C_DesignId_016 */
/* Requirements : HL_SR294 */
void i2cSetStop(i2cBASE_t *i2c)
{
/* USER CODE BEGIN (9) */
/* USER CODE END */
i2c->MDR |= (uint32)I2C_STOP_COND; /* generate stop condition */
/* USER CODE BEGIN (10) */
/* USER CODE END */
}
/** @fn void i2cSetCount(i2cBASE_t *i2c,uint32 cnt)
* @brief Set i2c data count
* @param[in] i2c - i2c module base address
* @param[in] cnt - data count
* Set i2c count to a transfer value after which the stop condition needs to be generated.
* (Only in Master Mode)
*/
/* SourceId : I2C_SourceId_007 */
/* DesignId : I2C_DesignId_017 */
/* Requirements : HL_SR295 */
void i2cSetCount(i2cBASE_t *i2c ,uint32 cnt)
{
/* USER CODE BEGIN (11) */
/* USER CODE END */
i2c->CNT = cnt; /* set i2c count */
/* USER CODE BEGIN (12) */
/* USER CODE END */
}
/** @fn uint32 i2cIsTxReady(i2cBASE_t *i2c)
* @brief Check if Tx buffer empty
* @param[in] i2c - i2c module base address
*
* @return The TX ready flag
*
* Checks to see if the Tx buffer ready flag is set, returns
* 0 is flags not set otherwise will return the Tx flag itself.
*/
/* SourceId : I2C_SourceId_008 */
/* DesignId : I2C_DesignId_005 */
/* Requirements : HL_SR283 */
uint32 i2cIsTxReady(i2cBASE_t *i2c)
{
/* USER CODE BEGIN (13) */
/* USER CODE END */
return i2c->STR & (uint32)I2C_TX_INT;
/* USER CODE BEGIN (14) */
/* USER CODE END */
}
/** @fn void i2cSendByte(i2cBASE_t *i2c, uint8 byte)
* @brief Send Byte
* @param[in] i2c - i2c module base address
* @param[in] byte - byte to transfer
*
* Sends a single byte in polling mode, will wait in the
* routine until the transmit buffer is empty before sending
* the byte. Use i2cIsTxReady to check for Tx buffer empty
* before calling i2cSendByte to avoid waiting.
*/
/* SourceId : I2C_SourceId_009 */
/* DesignId : I2C_DesignId_006 */
/* Requirements : HL_SR284 */
void i2cSendByte(i2cBASE_t *i2c, uint8 byte)
{
/* USER CODE BEGIN (15) */
/* USER CODE END */
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "Potentially infinite loop found - Hardware Status check for execution sequence" */
while ((i2c->STR & (uint32)I2C_TX_INT) == 0U)
{
} /* Wait */
i2c->DXR = (uint32)byte;
/* USER CODE BEGIN (16) */
/* USER CODE END */
}
/** @fn void i2cSend(i2cBASE_t *i2c, uint32 length, uint8 * data)
* @brief Send Data
* @param[in] i2c - i2c module base address
* @param[in] length - number of data words to transfer
* @param[in] data - pointer to data to send
*
* Send a block of data pointed to by 'data' and 'length' bytes
* long. If interrupts have been enabled the data is sent using
* interrupt mode, otherwise polling mode is used. In interrupt
* mode transmission of the first byte is started and the routine
* returns immediately, i2cSend must not be called again until the
* transfer is complete, when the i2cNotification callback will
* be called. In polling mode, i2cSend will not return until
* the transfer is complete.
*
* @note if data word is less than 8 bits, then the data must be left
* aligned in the data byte.
*/
/* SourceId : I2C_SourceId_010 */
/* DesignId : I2C_DesignId_007 */
/* Requirements : HL_SR285 */
void i2cSend(i2cBASE_t *i2c, uint32 length, uint8 * data)
{
/* USER CODE BEGIN (17) */
/* USER CODE END */
if ((g_i2cTransfer_t.mode & (uint32)I2C_TX_INT) != 0U)
{
/* Interrupt mode */
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
g_i2cTransfer_t.data = data;
/* start transmit by sending first byte */
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
i2c->DXR = (uint32)(*g_i2cTransfer_t.data);
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
/*SAFETYMCUSW 567 S MR:17.1,17.4 <APPROVED> "Pointer increment needed" */
g_i2cTransfer_t.data++;
/* Length -1 since one data is written already */
g_i2cTransfer_t.length = (length - 1U);
/* Enable Transmit Interrupt */
i2c->IMR |= (uint32)I2C_TX_INT;
}
else
{
/* send the data */
while (length > 0U)
{
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "Potentially infinite loop found - Hardware Status check for execution sequence" */
while ((i2c->STR & (uint32)I2C_TX_INT) == 0U)
{
} /* Wait */
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
i2c->DXR = (uint32)(*data);
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
/*SAFETYMCUSW 567 S MR:17.1,17.4 <APPROVED> "Pointer increment needed" */
data++;
length--;
}
}
/* USER CODE BEGIN (18) */
/* USER CODE END */
}
/** @fn uint32 i2cIsRxReady(i2cBASE_t *i2c)
* @brief Check if Rx buffer full
* @param[in] i2c - i2c module base address
*
* @return The Rx ready flag
*
* Checks to see if the Rx buffer full flag is set, returns
* 0 is flags not set otherwise will return the Rx flag itself.
*/
/* SourceId : I2C_SourceId_011 */
/* DesignId : I2C_DesignId_008 */
/* Requirements : HL_SR286 */
uint32 i2cIsRxReady(i2cBASE_t *i2c)
{
/* USER CODE BEGIN (19) */
/* USER CODE END */
return i2c->STR & (uint32)I2C_RX_INT;
/* USER CODE BEGIN (20) */
/* USER CODE END */
}
/** @fn uint32 i2cIsStopDetected(i2cBASE_t *i2c)
* @brief Check if Stop Condition Detected
* @param[in] i2c - i2c module base address
*
* @return The Stop Condition Detected flag
*
* Checks to see if the Stop Condition Detected flag is set,
* returns 0 if flags not set otherwise will return the Stop
* Condition Detected flag itself.
*/
/* SourceId : I2C_SourceId_023 */
/* DesignId : I2C_DesignId_023 */
/* Requirements : HL_SR539 */
uint32 i2cIsStopDetected(i2cBASE_t *i2c)
{
return i2c->STR & (uint32)I2C_SCD_INT;
}
/** @fn uint32 i2cRxError(i2cBASE_t *i2c)
* @brief Return Rx Error flags
* @param[in] i2c - i2c module base address
*
* @return The Rx error flags
*
* Returns the Rx framing, overrun and parity errors flags,
* also clears the error flags before returning.
*/
/* SourceId : I2C_SourceId_012 */
/* DesignId : I2C_DesignId_010 */
/* Requirements : HL_SR288 */
uint32 i2cRxError(i2cBASE_t *i2c)
{
uint32 status = i2c->STR & ((uint32)I2C_AL_INT | (uint32)I2C_NACK_INT);
/* USER CODE BEGIN (21) */
/* USER CODE END */
i2c->STR = (uint32)((uint32)I2C_AL_INT | (uint32)I2C_NACK_INT);
/* USER CODE BEGIN (22) */
/* USER CODE END */
return status;
}
/** @fn void i2cClearSCD(i2cBASE_t *i2c)
* @brief Clears the Stop condition detect flags.
* @param[in] i2c - i2c module base address
*
* This function is called to clear the Stop condition detect(SCD) flag
*/
/* SourceId : I2C_SourceId_013 */
/* DesignId : I2C_DesignId_009 */
/* Requirements : HL_SR287 */
void i2cClearSCD(i2cBASE_t *i2c)
{
/* USER CODE BEGIN (23) */
/* USER CODE END */
i2c->STR = (uint32)I2C_SCD_INT;
/* USER CODE BEGIN (24) */
/* USER CODE END */
}
/** @fn uint8 i2cReceiveByte(i2cBASE_t *i2c)
* @brief Receive Byte
* @param[in] i2c - i2c module base address
*
* @return Received byte
*
* Receives a single byte in polling mode. If there is
* not a byte in the receive buffer the routine will wait
* until one is received. Use i2cIsRxReady to check to
* see if the buffer is full to avoid waiting.
*/
/* SourceId : I2C_SourceId_014 */
/* DesignId : I2C_DesignId_011 */
/* Requirements : HL_SR289 */
uint8 i2cReceiveByte(i2cBASE_t *i2c)
{
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "Potentially infinite loop found - Hardware Status check for execution sequence" */
while ((i2c->STR & (uint32)I2C_RX_INT) == 0U)
{
} /* Wait */
/* USER CODE BEGIN (25) */
/* USER CODE END */
return ((uint8)i2c->DRR);
}
/** @fn void i2cReceive(i2cBASE_t *i2c, uint32 length, uint8 * data)
* @brief Receive Data
* @param[in] i2c - i2c module base address
* @param[in] length - number of data words to transfer
* @param[in] data - pointer to data buffer
*
* Receive a block of 'length' bytes long and place it into the
* data buffer pointed to by 'data'. If interrupts have been
* enabled the data is received using interrupt mode, otherwise
* polling mode is used. In interrupt mode receive is setup and
* the routine returns immediately, i2cReceive must not be called
* again until the transfer is complete, when the i2cNotification
* callback will be called. In polling mode, i2cReceive will not
* return until the transfer is complete.
*/
/* SourceId : I2C_SourceId_015 */
/* DesignId : I2C_DesignId_012 */
/* Requirements : HL_SR290 */
void i2cReceive(i2cBASE_t *i2c, uint32 length, uint8 * data)
{
/* USER CODE BEGIN (26) */
/* USER CODE END */
if ((i2c->IMR & (uint32)I2C_RX_INT) != 0U)
{
/* we are in interrupt mode */
/* clear error flags */
i2c->STR = (uint32)I2C_AL_INT | (uint32)I2C_NACK_INT;
g_i2cTransfer_t.length = length;
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
g_i2cTransfer_t.data = data;
}
else
{
while (length > 0U)
{
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "Potentially infinite loop found - Hardware Status check for execution sequence" */
while ((i2c->STR & (uint32)I2C_RX_INT) == 0U)
{
} /* Wait */
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
*data = ((uint8)i2c->DRR);
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
/*SAFETYMCUSW 567 S MR:17.1,17.4 <APPROVED> "Pointer increment needed" */
data++;
length--;
}
}
/* USER CODE BEGIN (27) */
/* USER CODE END */
}
/** @fn void i2cEnableLoopback(i2cBASE_t *i2c)
* @brief Enable Loopback mode for self test
* @param[in] i2c - i2c module base address
*
* This function enables the Loopback mode for self test.
*/
/* SourceId : I2C_SourceId_016 */
/* DesignId : I2C_DesignId_018 */
/* Requirements : HL_SR296 */
void i2cEnableLoopback(i2cBASE_t *i2c)
{
/* USER CODE BEGIN (28) */
/* USER CODE END */
/* enable digital loopback */
i2c->MDR |= ((uint32)1U << 6U);
/* USER CODE BEGIN (29) */
/* USER CODE END */
}
/** @fn void i2cDisableLoopback(i2cBASE_t *i2c)
* @brief Enable Loopback mode for self test
* @param[in] i2c - i2c module base address
*
* This function disable the Loopback mode.
*/
/* SourceId : I2C_SourceId_017 */
/* DesignId : I2C_DesignId_019 */
/* Requirements : HL_SR297 */
void i2cDisableLoopback(i2cBASE_t *i2c)
{
/* USER CODE BEGIN (30) */
/* USER CODE END */
/* Disable Loopback Mode */
i2c->MDR &= 0xFFFFFFBFU;
/* USER CODE BEGIN (31) */
/* USER CODE END */
}
/** @fn i2cEnableNotification(i2cBASE_t *i2c, uint32 flags)
* @brief Enable interrupts
* @param[in] i2c - i2c module base address
* @param[in] flags - Interrupts to be enabled, can be ored value of:
* i2c_FE_INT - framing error,
* i2c_OE_INT - overrun error,
* i2c_PE_INT - parity error,
* i2c_RX_INT - receive buffer ready,
* i2c_TX_INT - transmit buffer ready,
* i2c_WAKE_INT - wakeup,
* i2c_BREAK_INT - break detect
*/
/* SourceId : I2C_SourceId_018 */
/* DesignId : I2C_DesignId_013 */
/* Requirements : HL_SR291 */
void i2cEnableNotification(i2cBASE_t *i2c, uint32 flags)
{
/* USER CODE BEGIN (32) */
/* USER CODE END */
g_i2cTransfer_t.mode |= (flags & (uint32)I2C_TX_INT);
i2c->IMR = (flags & (uint32)(~(uint32)I2C_TX_INT));
}
/** @fn i2cDisableNotification(i2cBASE_t *i2c, uint32 flags)
* @brief Disable interrupts
* @param[in] i2c - i2c module base address
* @param[in] flags - Interrupts to be disabled, can be ored value of:
* i2c_FE_INT - framing error,
* i2c_OE_INT - overrun error,
* i2c_PE_INT - parity error,
* i2c_RX_INT - receive buffer ready,
* i2c_TX_INT - transmit buffer ready,
* i2c_WAKE_INT - wakeup,
* i2c_BREAK_INT - break detect
*/
/* SourceId : I2C_SourceId_019 */
/* DesignId : I2C_DesignId_014 */
/* Requirements : HL_SR292 */
void i2cDisableNotification(i2cBASE_t *i2c, uint32 flags)
{
uint32 int_mask;
/* USER CODE BEGIN (33) */
/* USER CODE END */
g_i2cTransfer_t.mode &= (uint32)(~(flags & (uint32)I2C_TX_INT));
int_mask = i2c->IMR &(uint32)(~(uint32)(flags | (uint32)I2C_TX_INT));
i2c->IMR = int_mask;
}
/** @fn i2cSetMode(i2cBASE_t *i2c, uint32 mode)
* @brief Sets Master or Slave mode.
* @param[in] i2c - i2c module base address
* @param[in] mode - Mode can be either:
* I2C_MASTER - Master Mode,
* I2C_SLAVE - Slave Mode
*/
/* SourceId : I2C_SourceId_020 */
/* DesignId : I2C_DesignId_024 */
/* Requirements : HL_SR526 */
void i2cSetMode(i2cBASE_t *i2c, uint32 mode)
{
uint32 temp_mdr;
/* USER CODE BEGIN (34) */
/* USER CODE END */
/* set Master or Slave Mode */
temp_mdr = (i2c->MDR & (~I2C_MASTER));
i2c->MDR = (temp_mdr | mode);
/* USER CODE BEGIN (35) */
/* USER CODE END */
}
/** @fn void i2cGetConfigValue(i2c_config_reg_t *config_reg, config_value_type_t type)
* @brief Get the initial or current values of the I2C configuration registers
*
* @param[in] *config_reg: pointer to the struct to which the initial or current
* value of the configuration registers need to be stored
* @param[in] type: whether initial or current value of the configuration registers need to be stored
* - InitialValue: initial value of the configuration registers will be stored
* in the struct pointed by config_reg
* - CurrentValue: initial value of the configuration registers will be stored
* in the struct pointed by config_reg
*
* This function will copy the initial or current value (depending on the parameter 'type')
* of the configuration registers to the struct pointed by config_reg
*
*/
/* SourceId : I2C_SourceId_021 */
/* DesignId : I2C_DesignId_021 */
/* Requirements : HL_SR300 */
void i2cGetConfigValue(i2c_config_reg_t *config_reg, config_value_type_t type)
{
if (type == InitialValue)
{
config_reg->CONFIG_OAR = I2C_OAR_CONFIGVALUE;
config_reg->CONFIG_IMR = I2C_IMR_CONFIGVALUE;
config_reg->CONFIG_CLKL = I2C_CLKL_CONFIGVALUE;
config_reg->CONFIG_CLKH = I2C_CLKH_CONFIGVALUE;
config_reg->CONFIG_CNT = I2C_CNT_CONFIGVALUE;
config_reg->CONFIG_SAR = I2C_SAR_CONFIGVALUE;
config_reg->CONFIG_MDR = I2C_MDR_CONFIGVALUE;
config_reg->CONFIG_EMDR = I2C_EMDR_CONFIGVALUE;
config_reg->CONFIG_PSC = I2C_PSC_CONFIGVALUE;
config_reg->CONFIG_DMAC = I2C_DMAC_CONFIGVALUE;
config_reg->CONFIG_FUN = I2C_FUN_CONFIGVALUE;
config_reg->CONFIG_DIR = I2C_DIR_CONFIGVALUE;
config_reg->CONFIG_ODR = I2C_ODR_CONFIGVALUE;
config_reg->CONFIG_PD = I2C_PD_CONFIGVALUE;
config_reg->CONFIG_PSL = I2C_PSL_CONFIGVALUE;
}
else
{
/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
config_reg->CONFIG_OAR = i2cREG1->OAR;
config_reg->CONFIG_IMR = i2cREG1->IMR;
config_reg->CONFIG_CLKL = i2cREG1->CKL;
config_reg->CONFIG_CLKH = i2cREG1->CKH;
config_reg->CONFIG_CNT = i2cREG1->CNT;
config_reg->CONFIG_SAR = i2cREG1->SAR;
config_reg->CONFIG_MDR = i2cREG1->MDR;
config_reg->CONFIG_EMDR = i2cREG1->EMDR;
config_reg->CONFIG_PSC = i2cREG1->PSC;
config_reg->CONFIG_DMAC = i2cREG1->DMACR;
config_reg->CONFIG_FUN = i2cREG1->PFNC;
config_reg->CONFIG_DIR = i2cREG1->DIR;
config_reg->CONFIG_ODR = i2cREG1->PDR;
config_reg->CONFIG_PD = i2cREG1->PDIS;
config_reg->CONFIG_PSL = i2cREG1->PSEL;
}
}
/** @fn i2cSetDirection(i2cBASE_t *i2c, uint32 dir)
* @brief Sets I2C as transmitter or receiver.
* @param[in] i2c - i2c module base address
* @param[in] dir - This can be one of the following:
* I2C_TRANSMITTER - Transmit Mode,
* I2C_RECEIVER - Receive Mode
*/
/* SourceId : I2C_SourceId_024 */
/* DesignId : I2C_DesignId_020 */
/* Requirements : HL_SR540 */
void i2cSetDirection(i2cBASE_t *i2c, uint32 dir)
{
/* USER CODE BEGIN (47) */
/* USER CODE END */
/* set Transmit/Receive mode */
i2c->MDR &= ~I2C_TRANSMITTER;
i2c->MDR |= dir;
/* USER CODE BEGIN (48) */
/* USER CODE END */
}
/** @fn i2cIsMasterReady(i2cBASE_t *i2c)
* @brief Indicates whether MST bit is set or cleared to indicate that stop
* condition was generated. This API should be called after Master Tx or Rx
* to check if the transaction is complete.
* @param[in] i2c - i2c module base address
* @return boolean value to indicate whether MST bit is cleared after STOP bit is generated.
* - TRUE, if MST bit is cleared.
* - FALSE, if MST bit is set.
*/
/* SourceId : I2C_SourceId_025 */
/* DesignId : I2C_DesignId_025 */
/* Requirements : HL_SR541 */
bool i2cIsMasterReady(i2cBASE_t *i2c)
{
bool retVal = 0U;
/* USER CODE BEGIN (49) */
/* USER CODE END */
/* check if MST bit is cleared. */
if((i2c->MDR & I2C_MASTER) == 0)
{
retVal = true;
}
else
{
retVal = false;
}
return retVal;
/* USER CODE BEGIN (50) */
/* USER CODE END */
}
/** @fn i2cIsBusBusy(i2cBASE_t *i2c)
* @brief Returns the state of the bus busy flag. True if it is set and false otherwise.
* @param[in] i2c - i2c module base address
* @return boolean value to indicate whether BB bit is set in the status register.
* - TRUE, if BB bit is set.
* - FALSE, if BB bit is cleared.
*/
/* SourceId : I2C_SourceId_026 */
/* DesignId : I2C_DesignId_026 */
/* Requirements : HL_SR542 */
bool i2cIsBusBusy(i2cBASE_t *i2c)
{
bool retVal = 0U;
/* USER CODE BEGIN (51) */
/* USER CODE END */
/* check if BB bit is set. */
if((i2c->STR & I2C_BUSBUSY) == I2C_BUSBUSY)
{
retVal = true;
}
else
{
retVal = false;
}
return retVal;
/* USER CODE BEGIN (52) */
/* USER CODE END */
}
#include "i2c_lcd.h"
#include "i2c.h"
extern void delay(uint32);
void lcd_send_cmd(I2C_LCD_HandleTypeDef *lcd, char cmd) {
char upper = (cmd & 0xF0);
char lower = ((cmd << 4) & 0xF0);
uint8_t data_t[4] = {
upper | 0x0C, upper | 0x08,
lower | 0x0C, lower | 0x08
};
i2cSetSlaveAdd(lcd->i2c, lcd->address);
i2cSetDirection(lcd->i2c, I2C_TRANSMITTER);
i2cSetCount(lcd->i2c, 4);
i2cSetMode(lcd->i2c, I2C_MASTER);
i2cSetStart(lcd->i2c);
i2cSend(lcd->i2c, 4, data_t);
while(i2cIsStopDetected(lcd->i2c) == false);
}
void lcd_send_cmd_AUEHSIM(I2C_LCD_HandleTypeDef *lcd, char cmd) {
char upper = (cmd & 0xF0);
char lower = ((cmd << 4) & 0xF0);
uint8_t data_t[4] = {
upper | 0x0C, upper | 0x08,
lower | 0x0C, lower | 0x08
};
i2cSetSlaveAdd(lcd->i2c, lcd->address);
i2cSetDirection(lcd->i2c, I2C_TRANSMITTER);
i2cSetCount(lcd->i2c, 4);
i2cSetMode(lcd->i2c, I2C_MASTER);
i2cSetStop(lcd->i2c);//auehsim
i2cSetStart(lcd->i2c);
i2cSend(lcd->i2c, 4, data_t);
/* Wait until Bus Busy is cleared */
while(i2cIsBusBusy(lcd->i2c) == true);
/* Wait until Stop is detected */
while(i2cIsStopDetected(lcd->i2c) == 0);
/* Clear the Stop condition */
i2cClearSCD(lcd->i2c);
}
void lcd_send_data(I2C_LCD_HandleTypeDef *lcd, char data) {
char upper = (data & 0xF0);
char lower = ((data << 4) & 0xF0);
uint8_t data_t[4] = {
upper | 0x0D, upper | 0x09,
lower | 0x0D, lower | 0x09
};
i2cSetSlaveAdd(lcd->i2c, lcd->address);
i2cSetDirection(lcd->i2c, I2C_TRANSMITTER);
i2cSetCount(lcd->i2c, 4);
i2cSetMode(lcd->i2c, I2C_MASTER);
i2cSetStart(lcd->i2c);
i2cSend(lcd->i2c, 4, data_t);
while(i2cIsStopDetected(lcd->i2c) == false);
}
void lcd_init(I2C_LCD_HandleTypeDef *lcd) {
delay(50);
lcd_send_cmd(lcd, 0x30); delay(5);
lcd_send_cmd(lcd, 0x30); delay(1);
lcd_send_cmd(lcd, 0x30); delay(10);
lcd_send_cmd(lcd, 0x20); delay(10);
lcd_send_cmd(lcd, 0x28); delay(1);
lcd_send_cmd(lcd, 0x08); delay(1);
lcd_send_cmd(lcd, 0x01); delay(2);
lcd_send_cmd(lcd, 0x06); delay(1);
lcd_send_cmd(lcd, 0x0C);
}
void lcd_init_AUEHSIM(I2C_LCD_HandleTypeDef *lcd) {
delay(50);// Wait for LCD power-up
lcd_send_cmd_AUEHSIM(lcd, 0x30); // Wake up command
delay(5);
lcd_send_cmd_AUEHSIM(lcd, 0x30);// Wake up command
delay(1);
lcd_send_cmd_AUEHSIM(lcd, 0x30);// Wake up command
delay(10);
lcd_send_cmd_AUEHSIM(lcd, 0x20);//Set to 4-bit mode
delay(10);
lcd_send_cmd_AUEHSIM(lcd, 0x28);// 4-bit mode, 2 lines, 5x8 font
delay(1);
lcd_send_cmd_AUEHSIM(lcd, 0x08);// Display off, cursor off, blink off
delay(1);
lcd_send_cmd_AUEHSIM(lcd, 0x01);// Clear display
delay(2);
lcd_send_cmd_AUEHSIM(lcd, 0x06);// Entry mode: cursor moves right
delay(1);
lcd_send_cmd_AUEHSIM(lcd, 0x0C);// Display on, cursor off, blink off
}
void lcd_clear(I2C_LCD_HandleTypeDef *lcd)
{
uint8_t i=0;
lcd_send_cmd(lcd, 0x80); // Move cursor to the home position
// Clear all characters
// 16x4 = 64 characters
// 20x4 = 80 characters
// So 80 character clearing is enough for both 16x2, 16x4, 20x2 and 20x5 displays
for (i = 0; i < 80; i++)
{
lcd_send_data(lcd, ' '); // Write a space on each position
}
}
void lcd_puts(I2C_LCD_HandleTypeDef *lcd, char *str) {
while (*str) lcd_send_data(lcd, *str++);
}
/** @file sys_main.c
* @brief Application main file
* @date 11-Dec-2018
* @version 04.07.01
*
* This file contains an empty main function,
* which can be used for the application.
*/
/*
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "sys_common.h"
/* USER CODE BEGIN (1) */
#include "system.h"
#include "i2c.h"
#include "i2c_lcd.h"
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
void delay(uint32 delay_ms) {
uint32 i, j;
for (i = 0; i < delay_ms * 1000; i++) {
for (j = 0; j < 5; j++);
}
}
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
i2cInit();
/* LCD yap land rmas */
I2C_LCD_HandleTypeDef lcd;
lcd.i2c = i2cREG1;
lcd.address = 0x4E; // PCF8574A I2C addres (0x27 << 1)
/* LCD'yi ba lat */
lcd_init_AUEHSIM(&lcd);
lcd_clear(&lcd);//auehsim
/* LCD'ye mesaj yaz */
lcd_puts(&lcd, "Merhaba TMS570");
/* Ana d ng */
while(1) {
lcd_send_cmd(&lcd, 0xC0); // kinci sat ra git
lcd_puts(&lcd, "I2C LCD calisti");
delay(1000);
lcd_send_cmd(&lcd, 0x01); // Ekran temizle
delay(1000);
lcd_puts(&lcd, "Merhaba TMS570");
}
/* USER CODE END */
return 0;
}
/* USER CODE BEGIN (4) */
/* USER CODE END */
sys_main.c
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "sys_common.h"
/* USER CODE BEGIN (1) */
#include "system.h"
#include "i2c.h"
#include "i2c_lcd.h"
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
void delay(uint32 delay_ms) {
uint32 i, j;
for (i = 0; i < delay_ms * 1000; i++) {
for (j = 0; j < 5; j++);
}
}
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
i2cInit();
/* LCD yap */
I2C_LCD_HandleTypeDef lcd;
lcd.i2c = i2cREG1;
lcd.address = 0x4E; // PCF8574A I2C addres (0x27 << 1)
/* LCD'yi ba lat */
lcd_init_AUEHSIM(&lcd); // I am having problem inside the lcd_init_AUEHSIM(&lcd)
lcd_clear(&lcd);//auehsim
/* LCD'ye mesaj yaz */
lcd_puts(&lcd, "Merhaba TMS570");
/* Ana d ng */
while(1) {
lcd_send_cmd(&lcd, 0xC0); // kinci sat ra git
lcd_puts(&lcd, "I2C LCD calisti");
delay(1000);
lcd_send_cmd(&lcd, 0x01); // Ekran temizle
delay(1000);
lcd_puts(&lcd, "Merhaba TMS570");
}
/* USER CODE END */
return 0;
}
i2c_lcd.c
#include "i2c_lcd.h"
#include "i2c.h"
extern void delay(uint32);
void lcd_init_AUEHSIM(I2C_LCD_HandleTypeDef *lcd) { // When I call lcd_init_AUEHSIM(&lcd); code comes here.
delay(50);// Wait for LCD power-up
lcd_send_cmd_AUEHSIM(lcd, 0x30); // Wake up command // It never comes out of the first lcd_send_cmd_AUEHSIM(lcd, 0x30); function.
delay(5);
lcd_send_cmd_AUEHSIM(lcd, 0x30);// Wake up command
delay(1);
lcd_send_cmd_AUEHSIM(lcd, 0x30);// Wake up command
delay(10);
lcd_send_cmd_AUEHSIM(lcd, 0x20);//Set to 4-bit mode
delay(10);
lcd_send_cmd_AUEHSIM(lcd, 0x28);// 4-bit mode, 2 lines, 5x8 font
delay(1);
lcd_send_cmd_AUEHSIM(lcd, 0x08);// Display off, cursor off, blink off
delay(1);
lcd_send_cmd_AUEHSIM(lcd, 0x01);// Clear display
delay(2);
lcd_send_cmd_AUEHSIM(lcd, 0x06);// Entry mode: cursor moves right
delay(1);
lcd_send_cmd_AUEHSIM(lcd, 0x0C);// Display on, cursor off, blink off
}
void lcd_send_cmd_AUEHSIM(I2C_LCD_HandleTypeDef *lcd, char cmd) { // When I call lcd_send_cmd_AUEHSIM(lcd, 0x30); code comes here.
char upper = (cmd & 0xF0);
char lower = ((cmd << 4) & 0xF0);
uint8_t data_t[4] = {
upper | 0x0C, upper | 0x08,
lower | 0x0C, lower | 0x08
};
i2cSetSlaveAdd(lcd->i2c, lcd->address);
i2cSetDirection(lcd->i2c, I2C_TRANSMITTER);
i2cSetCount(lcd->i2c, 4);
i2cSetMode(lcd->i2c, I2C_MASTER);
i2cSetStop(lcd->i2c);//auehsim
i2cSetStart(lcd->i2c);
i2cSend(lcd->i2c, 4, data_t); // I believe the main problem is inside i2cSend(lcd->i2c, 4, data_t); function. Because when it goes in i2cSend it stays in an infinite loop.
/* Wait until Bus Busy is cleared */
while(i2cIsBusBusy(lcd->i2c) == true);
/* Wait until Stop is detected */
while(i2cIsStopDetected(lcd->i2c) == 0);
/* Clear the Stop condition */
i2cClearSCD(lcd->i2c);
}
i2c.c
void i2cSend(i2cBASE_t *i2c, uint32 length, uint8 * data)
{
/* USER CODE BEGIN (17) */
/* USER CODE END */
if ((g_i2cTransfer_t.mode & (uint32)I2C_TX_INT) != 0U)
{
/* Interrupt mode */
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
g_i2cTransfer_t.data = data;
/* start transmit by sending first byte */
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
i2c->DXR = (uint32)(*g_i2cTransfer_t.data);
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
/*SAFETYMCUSW 567 S MR:17.1,17.4 <APPROVED> "Pointer increment needed" */
g_i2cTransfer_t.data++;
/* Length -1 since one data is written already */
g_i2cTransfer_t.length = (length - 1U);
/* Enable Transmit Interrupt */
i2c->IMR |= (uint32)I2C_TX_INT;
}
else
{
/* send the data */
while (length > 0U)
{
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "Potentially infinite loop found - Hardware Status check for execution sequence" */
while ((i2c->STR & (uint32)I2C_TX_INT) == 0U) // Stays in this infinite loop.
{
} /* Wait */
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
i2c->DXR = (uint32)(*data);
/*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
/*SAFETYMCUSW 567 S MR:17.1,17.4 <APPROVED> "Pointer increment needed" */
data++;
length--;
}
}
/* USER CODE BEGIN (18) */
/* USER CODE END */
}