Part Number: AM263P4-Q1
Other Parts Discussed in Thread: OPA4350, , AM263P4, REF35
Tool/software:
Hi All,
We are considering using an external ADC voltage reference with AM263P4-Q1. I've looked at the schematic for the AM263P4 control card that uses a pair of OPA4350 opamps to buffer the external reference. But I still have a few questions below:
1. Is the capacitance recommended for the Vref pins in the datasheet (4.7uF + 0.1uF + 0.1uF) still recommended when using an external reference, or can we go much lower? The reason to reduce capacitance is to help with stability of the external buffer. Even a "High Cload" opamp like OPA4350 only plots stability in the datasheet up to 1uF, and it gets fairly peak-y even there. Can we reduce the capacitance with an external buffer? Can we reduce it significantly (<10nF) and allow the external buffer to provide stability?
2. On the AM263P4 control card, separate opamps buffer the ADC references for VREF G0/G1 and VREF G2 respectively. The AM263P4-Q1 datasheet mentions these reference inputs must be separated when using the internal references since they don't have enough current drive to be shorted together. But when using an external reference like REF35180 that has significant current drive, can I short G1/G2/G3 together and drive them with one external reference? Or are there ADC performance reasons not to do this?