Part Number: SYSCONFIG
Tool/software:
Hi,
My customer try to perform following setting by using DDR configuration tool for AM64x.
"tCCD_L_ns" : 6.25
"tRRD_L_ns" : 6
On the other hand, customer will use DDR clock as 800MHz.
Then we have folllowing question.
Q1, Except tCCD_L_ns" and "tRRD_L_ns", there are another specs "tCCD_L_tck" and "tRRD_L_tck".
When user set descrepancy between these two, is there any problem ?
(Which setting is used to configration of register setting ?)
Ex. When user set "DDRSS.ddr4.config_dram_tRRD_L_ns= 6;" but "DDRSS.ddr4.config_dram_tRRD_L_tck" is set as default value (in default this value is "4").
Q2, It seems that there is no setting item related to "burst mode" on DDR configuration tool. Can't user set burst mode setting on DDR configuration tool ?
Best Regards,