Part Number: LP-AM243
Other Parts Discussed in Thread: UNIFLASH,
Tool/software:
Dear Sirs,
I am encountering some issues when trying to flash the AM243x LaunchPad. I have already tried the following three methods:
- Using Windows Command Line with Boot Mode : UART mode
- I edited the default_sbl_ospi.cfg file to specify the required appimage.hs_fs and appimage_xip.
- Then I ran the following command:
"python uart_uniflash.py -p COM8 --cfg=sbl_prebuilt/am243x-lp/default_sbl_ospi.cfg" - However, I got the following error:

- I edited the default_sbl_ospi.cfg file to specify the required appimage.hs_fs and appimage_xip.
- Using UniFlash Tool with Configuration set to "AM243X (SERIAL)" and Boot Mode is also UART mode
- Settings are shown below:


- The following error occurred:

- Settings are shown below:
- Using UniFlash Tool with Configuration set to "LP-AM243 (LaunchPad)" and Boot Mode set to DEV mode
- Settings are shown below:

- The following error occurred:

- Settings are shown below:
Is there any way to resolve this? Or could there be an issue with my flash?
Additional Information:
When the boot mode is set to QSPI Flash mode, I can see the following serial output:
Thank you,
Harry Chu