This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

*****

  • Hi,

    What kind of settings are you programming to the device?

    Does this still happen when flashing an example program?

    -Matthew

  • Hi,

    I started to get this error after ı enabled the IWDT.

    No specific settings on debug.

    Thanks

  • Hi,

    Could you let me know the value of the WDTDBGCTL register?

    -Matthew

  • Hi,

    I did not set this register. It is in reset value which is 0

    Bit Field Type Reset Description
    31-1 RESERVED R 0h
    0 FREE R/W 0h Free run control0h = The WDT freezes functionality while the CPU is Halted during debug and resumes when the CPU is active.1h = The WDT ignores the state of the CPU Halted debug state.


    My IWDT init code:

    DL_IWDT_setClockDivider(IWDT_INST, DL_IWDT_CLOCK_DIVIDE_4);
    DL_IWDT_setTimerPeriod(IWDT_INST, DL_IWDT_TIMER_PERIOD_12_BITS);
    
    DL_IWDT_enableModule(IWDT_INST);

    I use DL_IWDT_restart(IWDT_INST) to clear IWDT.

    Thanks

  • Hi,

    The original message seems to have been removed. Could you quickly summarize the issue again?

    -Matthew

  • Hi Matthew,

    My original question was:

    Hello,

    I am getting this error when I try to debug my project.

    Console Output:

    CORTEX_M0P: Error connecting to the target: (Error -6310) PRSC module failed to read a register. (Emulation package 20.0.0.3178)
    CS_DAP_0: Trouble Writing Register PWRAP_DPREC0: (Error -2131 @ 0x20400) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 20.0.0.3178)
    CS_DAP_0: GEL: Error while executing PWRAP_DPREC0 = 0x00120008: Target failed to write register PWRAP_DPREC0
    at PWRAP_DPREC0=0x00120008

    Only solution to this problem I found is mass erase. After mass erase I can debug once. On the second debug attempt I get the same error.

    Is there any other solution to this problem?

    Thanks

  • Does this happen when you flash a different program to the device? Such as an example? 

    Are you working on a launchpad or custom board?