Part Number: AM263P4-Q1
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi,
I am using AM263P LP. I want to run example code on MCU+ SDK for AM263P. Before I have run many project on this board without any problem. But i can't run any project at now.
For example, I imported gpio_input_interrupt_am263px-lp_r5fss0-0_nortos_ti-arm-clang project .When I click debug button, I encounter this error.
Cortex_R5_0: AM263Px
Cortex_R5_0: Board Selected : CC
Cortex_R5_0: Part Selected : Standard
Cortex_R5_0: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x40: (Error -1065 @ 0x40) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 20.0.0.3178)
Cortex_R5_0: File Loader: Verification failed: Target failed to write 0x00000000
Cortex_R5_0: GEL: File: C:\...\gpio_input_interrupt_am263px-lp_r5fss0-0_nortos_ti-arm-clang\Release\gpio_input_interrupt_am263px-lp_r5fss0-0_nortos_ti-arm-clang.out: Load failed.
Best Regards,
Burak