Part Number: TMDS243EVM
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
In the example enet_cpsw_est_am243x-evm_r5fss0-0_freertos_ti-arm-clang, I want to change it to press T to send 160 packets, so I change the ENETAPP_TEST_TX_PKT_CNT to 160U, but the serial port printing result is as follows
#-----------------------------------------------------------------------------#
# #
# DEFAULT CONFIGURATION FILE TO BE USED WITH THE FLASHWRITER SCRIPT #
# #
#-----------------------------------------------------------------------------#
#
# By default this config file,
# - points to pre-built flash writer, bootloader for this EVM
# - The application image points to relative path of the ipc echo application image for this EVM
# - Make sure this application is built before running this script
# - You can customized this config file to point to your own bootloader and/or application images
# - You can use --operation=flashverify if you just want to verify the flash contents and not flash the file.
#
# First point to sbl_uart_uniflash binary, which function's as a server to flash one or more files
--flash-writer=sbl_prebuilt/am243x-evm/sbl_uart_uniflash.release.hs_fs.tiimage
# Now send one or more files to flash or flashverify as needed. The order of sending files does not matter
# Program the OSPI PHY tuning attack vector
--operation=flash-phy-tuning-data
# When sending bootloader make sure to flash at offset 0x0. ROM expects bootloader at offset 0x0
--file=sbl_prebuilt/am243x-evm/sbl_ospi.release.hs_fs.tiimage --operation=flash --flash-offset=0x0
# When sending application image, make sure to flash at offset 0x80000 (default) or to whatever offset your bootloader is configured for
--file=../../examples/drivers/ipc/ipc_notify_echo/am243x-evm/system_freertos_nortos/ipc_notify_echo_system.release.appimage.hs_fs --operation=flash --flash-offset=0x80000
# send the XIP image for this application, no need to specify flash offset since flash offset is specified within the image itself
--file=../../examples/drivers/ipc/ipc_notify_echo/am243x-evm/system_freertos_nortos/ipc_notify_echo_system.release.appimage_xip --operation=flash-xip