Tool/software:
Hi TI support team,
I'm trying to use Tamagawa encoder instead of EnDAT with "examples\tidep_01032_dual_motor_drive\single_chip_servo\am243x-lp\r5fss0-0_nortos" in the "motor_control_sdk_am243x_09_02_00_09." But I can't.
I know that IEP clock is 300MHzi n single chip_servo, it is 200MHz in t"amagawa_diagnostic\single_channel\am243x-lp\r5fss0-0_freertos" on the other hand.
I am trying to change some parameters. In one setting, I could get right SDDF output value in the "gSddfChSamps". But callback function "pruEncoderIrqHandler" was executed only once, not repeatedly.
In another setting, callback function was executed repatedly. But value in gSddfChSamps is wrong, which is bigger than 2^18.
Could you please give me some advice?
Thanks in advance.
Best regards,
Dai