Part Number: MSP432E401Y
Other Parts Discussed in Thread: TM4C1294NCPDT
Tool/software:
Hi Team,
We are planning to design a option board (60mm x 60mm size) which is capable of signal processing using motor vibration sensor data from industrial field. This optional module will be connected to main processor board through UART. Please suggest a suitable controller solution, The controller should have below mentioned features. Currently we chosen MSP432E401Y and let us know is there any better options we have.
1) M4 or M7 core with DSP capability
2) Should support RTOS
3) Should support external SRAM and NAND flash
4) Should have USB and ethernet interface
5) Number of pins should be less than 200 (Space constrains are there in board)