Part Number: MSPM0G3107
Tool/software:
MSMPM0 SDK: 2.4.0.06
Just wondering if this is a mistake in the MCAN SDK
I'm confused why the data section of this struct is 64 uint16_t instead of 64 uint8_t

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSPM0G3107
Tool/software:
MSMPM0 SDK: 2.4.0.06
Just wondering if this is a mistake in the MCAN SDK
I'm confused why the data section of this struct is 64 uint16_t instead of 64 uint8_t

Hi,
Sorry, I do not fully understand your question. Which variable you are referring to should be uint8_t in this post?
Best regards,
Cash Hao