This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634-Q1: How to change the syscfg to higher version based on old version project.

Part Number: AM2634-Q1
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

Hi team,

I ask this for my customer. My customer used the CCS12.2 and syscfg 1.11 to develop their project.

Recently they want to add more function based on this project, and they want to connect the ADC1_IN1 to CMPSSA2

and I find in their current syscfg, it seems have bug in CMPSSA Low comparator module:

And in my 1.24 syscfg, I can choose the INL as the input of CMPSSA Low comparator module

So I suggest them to update the sysconfig from 1.11 to 1.24, and they have update it successfully

But when they open original syscfg file using 1.24 syscfg, it fails

1. How to solve it? 

2. Is the bug of syscfg 1.11?

BRs

Shuqing

  • Hi Shuqing,

    Upgrading the syscfg is only going to upgrade the tool.

    The feature update that you are looking for will need update of MCU PLUS SDK release version to 10.2

  • Now, in order to update the SDK, customers will need to rebuild their example, using the new SDK drivers. There will be build errors due to new functions and features. Also currently, you mentioned customer is using 8.0 version of MCU PLUS SDK, which is a significant change moving to 10.2