This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3519-Q1: What the algorithm of our hardware ECC?

Part Number: MSPM0G3519-Q1

Tool/software:

Hi team, 

I ask this for my customer. 

For DED, we have a register to restore which address have ECC error

But for SED, it isn't have this register. right?

In our datasheet, it shows every 64-bit flash word will generate 8-bit ECC code, and they want to know what the algorithm of our hardware ECC, they want to calculate it using software and compared to hardware ECC to check if this 64bit have ECC error.

BRs

Shuqing

  • For ECC calculation, please refer to this:

    #!/usr/bin/env python3
    #
    # Copyright (C) 2024-2025 Texas Instruments Incorporated - ALL RIGHTS RESERVED
    #
    # NOTE: requires python 3.10 or later to get bit_count
    
    import click
    
    
    class BasedIntParamType(click.ParamType):
        name = "integer"
    
        def convert(self, value, param, ctx):
            if isinstance(value, int):
                return value
    
            try:
                if value[:2].lower() == "0x":
                    return int(value[2:], 16)
                elif value[:1] == "0":
                    return int(value, 8)
                return int(value, 10)
            except ValueError:
                self.fail(f"{value!r} is not a valid integer", param, ctx)
    
    
    # bit 0 mask
    bit0_dataMask = 0xB4D1B4D14B2E4B2E
    bit0_addrMask = 0x2AA750
    
    # bit 1 mask
    bit1_dataMask = 0x1557155715571557
    bit1_addrMask = 0x5D688
    
    # bit 2 mask
    bit2_dataMask = 0xA699A699A699A699
    bit2_addrMask = 0x154DA8
    
    # bit 3 mask
    bit3_dataMask = 0x38E338E338E338E3
    bit3_addrMask = 0x353C68
    
    # bit 4 mask
    bit4_dataMask = 0xC0FCC0FCC0FCC0FC
    bit4_addrMask = 0xCFC18
    0x3FC000
    # bit 5 mask
    bit5_dataMask = 0xFF00FF00FF00FF00
    bit5_addrMask = 0x3FC00
    
    # bit 6 mask
    bit6_dataMask = 0xFF0000FFFF0000FF
    bit6_addrMask = 0x3FFC00
    
    # bit 7 mask
    bit7_dataMask = 0x00FFFF00FF0000FF
    bit7_addrMask = 0x3F8
    
    
    def calculate_ecc(data_in, addr_in):
        bit0_bitCount = (data_in & bit0_dataMask).bit_count() + (
            addr_in & bit0_addrMask
        ).bit_count()
        bit0 = (bit0_bitCount & 0x1) << 0
        bit1_bitCount = (data_in & bit1_dataMask).bit_count() + (
            addr_in & bit1_addrMask
        ).bit_count()
        bit1 = (bit1_bitCount & 0x1) << 1
        bit2_bitCount = (
            (data_in & bit2_dataMask).bit_count()
            + (addr_in & bit2_addrMask).bit_count()
            + 1
        )
        bit2 = (bit2_bitCount & 0x1) << 2
        bit3_bitCount = (
            (data_in & bit3_dataMask).bit_count()
            + (addr_in & bit3_addrMask).bit_count()
            + 1
        )
        bit3 = (bit3_bitCount & 0x1) << 3
        bit4_bitCount = (
            (data_in & bit4_dataMask).bit_count()
            + (addr_in & bit4_addrMask).bit_count()
            + 1
        )
        bit4 = (bit4_bitCount & 0x1) << 4
        bit5_bitCount = (
            (data_in & bit5_dataMask).bit_count()
            + (addr_in & bit5_addrMask).bit_count()
            + 1
        )
        bit5 = (bit5_bitCount & 0x1) << 5
        bit6_bitCount = (
            (data_in & bit6_dataMask).bit_count()
            + (addr_in & bit6_addrMask).bit_count()
            + 1
        )
        bit6 = (bit6_bitCount & 0x1) << 6
        bit7_bitCount = (
            (data_in & bit7_dataMask).bit_count()
            + (addr_in & bit7_addrMask).bit_count()
            + 1
        )
        bit7 = (bit7_bitCount & 0x1) << 7
    
        ecc = bit7 | bit6 | bit5 | bit4 | bit3 | bit2 | bit1 | bit0
    
        return ecc
    
    
    @click.command()
    @click.option(
        "--data",
        default=0xAAAAAAAAAAAAAAAA,
        type=BasedIntParamType(),
        help="64-bit data to be used as basis for CRC",
    )
    @click.option(
        "--addr",
        default=0x12000,
        type=BasedIntParamType(),
        help="starting address for flash writes",
    )
    def calculate_three_eccs(data, addr):
        ecc1 = calculate_ecc(data, addr)
        print("Addr: %x Ecc: %x " % (addr, ecc1))
        addr = addr + 8
        ecc2 = calculate_ecc(data, addr)
        print("Addr: %x Ecc: %x " % (addr, ecc2))
        addr = addr + 8
        ecc3 = calculate_ecc(data, addr)
        print("Addr: %x Ecc: %x " % (addr, ecc3))
    
    
    @click.command()
    @click.option(
        "--data",
        default=0xAAAAAAAAAAAAAAAA,
        type=BasedIntParamType(),
        help="64-bit data to be used as basis for CRC",
    )
    @click.option(
        "--addr",
        default=0x12000,
        type=BasedIntParamType(),
        help="starting address for flash writes",
    )
    def calculate_one_ecc(data, addr):
        ecc1 = calculate_ecc(data, addr)
        print("Addr: %x Ecc: %x " % (addr, ecc1))
        addr = addr + 8
    
    
    if __name__ == "__main__":
        calculate_three_eccs()