Part Number: MSPM0L2228
Tool/software:
Hi,
My customer reported VBAT power consumption is higher than expected with Rev.B part.
Please see below measurement results. Unit is [uA]. Red one is out of spec.
|
Temp |
Sample # |
Spec. |
||||
|
3 |
4 |
5 |
6 |
typ |
max |
|
|
-40℃ |
1.583 |
1.576 |
1.686 |
1.517 |
1.1 |
1.6 |
|
23℃ |
1.584 |
1.578 |
1.686 |
1.517 |
1.1 |
1.7 |
|
80℃ |
1.679 |
1.663 |
1.706 |
1.645 |
1.2 |
1.8 |
L2228 Datasheet:
There is a known bug (LFSS_ERR_01), but it is fixed in Rev.B. 
Thanks and regards,
Koichiro Tashiro