Part Number: TMDS243EVM
Tool/software:
Hello,
I have trouble with the pre-certification test:
Test Execution Log
| 1 | 09:58:51: DCP_1: Start of test DCP - DCP 1 without VLAN-Tag |
| 2 | 09:58:51: DCP_1: Test step 1: Requesting ResetToFactory (reset communication parameters) of the dut |
| 3 | 09:58:51: DCP_1: Test step 2: Waiting for the DUT to apply the reset to factory request. [ms]: 60000 |
| 4 | 09:59:51: DCP_1: Test step 3: Check the IdentifyAll response behavior. |
| 5 | 09:59:51: DCP_1: Test step 4: The requested IdentifyAll failed. |
| 6 | 09:59:51: Received an unexpected response block in a DCPIdentify.Res from type: OemDeviceId. |
| 7 | 09:59:51: DCP_1: Test step 4: DCP - DCP 1: Aborted due to errors. |
Could the problem be in the OemDeviceId item?
I analyzed the communications in Wireshark, and the VendorID and OemVendorID are different. I am using my own VendorID, but the OemVendorID is 0x1c4.
Where can I change the OemDeviceId?
Thank you in advance for your response.
Best regards, Vaclav V.