Part Number: MSPM0L1306
Tool/software:
The.txt file used for upgrading will generate the first 16 bytes according to the starting address set by the device_linker.cmd file when compiling, so it can only run on the set address. However, I set two partitions with two addresses, so how to generate only one.txt file after wiping through flash, It can run on both partition A and partition B.