Part Number: MCU-PLUS-SDK-AM273X
Tool/software:
Hello Support team,
I'm working on the AM273x EVM with MCU+ SDK. It seems to me that the MSS_SPIB mode setting in the example.syscfg of the sample mibspi_loopback project does not match with the actual SPI signals on J7 of EVM. I verified this with Saleae Logic 2.
For example, for AD7380-4 chipset, the SPI mode is 2 (CPOL = 1, CPHA = 0), in the AM273x .syscfg file I have to set to mode 3 (CPOL = 1, CPHA = 1).
Is there any reason for that? Or any suggestion?
Best regards,
Lin