Part Number: MSPM0L1306
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
I'm using LP-MSPM0L1306.
When trying to write software again after having written the software once, the following error occurs:
Filed to retrieve the Wait in Reset Mode: (Error -6311) PRSC module failed to write to a register.
When I perform a factory reset, the following error occurs:
CS_DAP_0: Trouble Reading Register SECAP_RCR: (Error -2131 @ 0x2020C) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 20.2.0.3536)
CS_DAP_0: GEL: Error while executing GEL_DAPInit_SECAPCommand(): Target failed to read register SECAP_RCR
at ('REG'::SECAP_RCR&0xFFFFU) [mspm0_cs_dap_init.gel:247]
at GEL_DAPInit_WaitForResponse() [mspm0_cs_dap_init.gel:426]
at GEL_DAPInit_SECAPCommand()
I can't write software or do a factory reset, so is there any solution?