This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2612: In OSPI(4s) -Quad Read Mode(Boot mode Pin: 0000), the program can't reboot from flash after enabling the watchdog.

Part Number: AM2612


Tool/software:

I have a custom flash with QSPI.

My custom board can boot form QSPI Flash( OSPI(4s) -Quad Read Mode)  after the device is powered on.

I sent a Modbus command to enable the watchdog on  the device. The program stopped running, but it didn't restart. 

This method of warm-restart via the watchdog works normally on the AM263X but abnormally on the AM261X.

Could you check why the program didn't restart?