Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello,
I want to wake up my MCU using a GPIO. I have configured GPIO PA12 for wake-up in the SysConfig file.
/**
* These arguments were used when this file was generated. They will be automatically applied on subsequent loads
* via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
* @cliArgs --device "MSPM0G350X" --part "Default" --package "LQFP-64(PM)" --product "mspm0_sdk@2.05.01.01"
* @v2CliArgs --device "MSPM0G3507" --package "LQFP-64(PM)" --product "mspm0_sdk@2.05.01.01"
* @versions {"tool":"1.24.0+4110"}
*/
/**
* Import the modules used in this configuration.
*/
const Board = scripting.addModule("/ti/driverlib/Board");
const GPIO = scripting.addModule("/ti/driverlib/GPIO", {}, false);
const GPIO1 = GPIO.addInstance();
const GPIO2 = GPIO.addInstance();
const RTC = scripting.addModule("/ti/driverlib/RTC");
const SYSCTL = scripting.addModule("/ti/driverlib/SYSCTL");
/**
* Write custom configuration values to the imported modules.
*/
GPIO1.$name = "GPIO_LEDS";
GPIO1.associatedPins.create(2);
GPIO1.associatedPins[0].assignedPort = "PORTA";
GPIO1.associatedPins[0].internalResistor = "PULL_UP";
GPIO1.associatedPins[0].$name = "USER_LED_1";
GPIO1.associatedPins[0].launchPadShortcut = "LED1En";
GPIO1.associatedPins[1].assignedPort = "PORTA";
GPIO1.associatedPins[1].assignedPortSegment = "Lower";
GPIO1.associatedPins[1].$name = "USER_TEST";
GPIO1.associatedPins[1].internalResistor = "PULL_UP";
GPIO1.associatedPins[1].pin.$assign = "PA15";
GPIO2.$name = "WakeUp";
GPIO2.port = "PORTA";
GPIO2.portSegment = "Lower";
GPIO2.associatedPins[0].$name = "PIN_0";
GPIO2.associatedPins[0].direction = "INPUT";
GPIO2.associatedPins[0].interruptEn = true;
GPIO2.associatedPins[0].internalResistor = "PULL_DOWN";
GPIO2.associatedPins[0].fastWakeEn = true;
GPIO2.associatedPins[0].polarity = "RISE";
GPIO2.associatedPins[0].pin.$assign = "PA12";
RTC.intervalAlarmEvent = "HOURCHANGE";
RTC.calDOW = "1";
RTC.calMin = 32;
RTC.calHour = 10;
RTC.calYear = 2021;
RTC.calMonth = "4";
RTC.calDOM = 5;
RTC.calAlarm1Min = 33;
RTC.calAlarm1Hour = 10;
RTC.calAlarm1DOW = "1";
RTC.calAlarm1DOM = 5;
RTC.calSec = 58;
RTC.enPerAlarm1 = true;
RTC.enabledInterrupts = ["PRESCALER1"];
SYSCTL.validateClkStatus = true;
SYSCTL.clockTreeEn = true;
SYSCTL.enableSleepOnExit = true;
SYSCTL.SYSOSC_Freq = 4000000;
SYSCTL.powerPolicy = "STANDBY0";
/**
* Pinmux solution for unlocked pins/peripherals. This ensures that minor changes to the automatic solver in a future
* version of the tool will not impact the pinmux you originally saw. These lines can be completely deleted in order to
* re-solve from scratch.
*/
Board.peripheral.$suggestSolution = "DEBUGSS";
Board.peripheral.swclkPin.$suggestSolution = "PA20";
Board.peripheral.swdioPin.$suggestSolution = "PA19";
GPIO1.associatedPins[0].pin.$suggestSolution = "PA0";
RTC.peripheral.$suggestSolution = "RTC";
Let me know the correction to implement the above.

Regrads,
Abhijeet D