Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Tool/software:
Hi - on tms570 HDK, we want to use one one HDK ( example HDK1) to do MibSPI comms with 4 other HDKs using MibSPI1,2, 3 and 5 as there is no MIb SPI available for channel 4. We want to also use MII for Ethernet comm with another device on HDK1. But Pin MUX in Halcogen, seems to have a conflict on G19 and R2 for MII and MibSPI thereby limiting to only two MibSPI channels ( 2 and 3) being available with MII. Although Halcogen shows U3 as default Option for MII, it is not available on the HDK? Is there another workaround/fix for this limitation?