Part Number: MSPM0C1104
Tool/software:
Hi,
We adopted XMSM0C1104S8YCJR with only 5 GPIO pins including PA19 & PA20 as SWDIO & SWCLK.
EE need more GPO and ask SW to re-configure PA19 & PA20 as GPO.
Nevertheless, we still need to flash the mcu by SWD.
Is it possible to configure these 2 pins as GPO and keep SWD to flash firmware at the same time?
FAE suggested us to as delay before GPIO init and it works.
But delay is not acceptable for user everytime device is turned on.