Part Number: TMS570LC4357
Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
Tool/software:
Hi Ibrahim,
Apologies for the delayed response! I was off for few days and didn't get time to work on this issue.
The TMS570LC4357 datasheet provides thermal resistance characteristics for the BGA package. These values, particularly the junction-to-board thermal resistance, are critical for calculating heat dissipation through conduction to the PCB in your vacuum environment.
On-Chip Temperature Monitoring
The TMS570LC4357 has three on-chip temperature sensors for monitoring the junction temperature. The measurements from these sensors are routed to a MibADC for conversion to digital values. This allows the application to monitor the device temperature and take action if it exceeds the specification. Possible actions include logging the event, turning off peripherals, or slowing down clocks to reduce the junction temperature.
During Single Event Latch-up (SEL) testing, the device was operated at an IC temperature of 125°C. The test was conducted with the kinetic energy of the ion specified for a vacuum environment. No latch-up events were observed under these conditions.
--
Thanks & regards,
Jagadish.