Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: How to test Profinet with LP-AM2434

Part Number: AM2434
Other Parts Discussed in Thread: DP83869

Tool/software:

Hello, TI expert:

       I am using  the ind_comms_sdk_am243x_11_00_00_12 to test profinet  stack protocol on the LP-AM2434, but the codesys profinet master can't scan the am2434 profinet slave.

I can't figure out where I went wrong.  I don't know what the default IP is for this version of the SDK( ind_comms_sdk_am243x_11_00_00_12 ). 

The serial port prints the following information. I'm not sure if the firmware failed to start properly?

[13:30:42.702]

[13:30:42.702] DMSC Firmware Version 11.0.7--v11.00.07 (Fancy Rat)

[13:30:42.709] DMSC Firmware revision 0xb

[13:30:42.709] DMSC ABI revision 4.0

[13:30:42.709]

[13:30:42.709] KPI_DATA: [BOOTLOADER_PROFILE] CPU Clock : 800.000 MHz

[13:30:42.802] KPI_DATA: [BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH

[13:30:42.802] KPI_DATA: [BOOTLOADER_PROFILE] Boot Media Clock : 100.000 MHz

[13:30:42.812] KPI_DATA: [BOOTLOADER_PROFILE] Boot Image Size : 295 KB

[13:30:42.822] KPI_DATA: [BOOTLOADER_PROFILE] Cores present :

[13:30:42.822] r5f0-0

[13:30:42.822] KPI_DATA: [BOOTLOADER PROFILE] SYSFW init : 11125us

[13:30:42.828] KPI_DATA: [BOOTLOADER PROFILE] System_init : 11709us

[13:30:42.872] KPI_DATA: [BOOTLOADER PROFILE] Drivers_open : 1645us

[13:30:42.872] KPI_DATA: [BOOTLOADER PROFILE] Board_driversOpen : 490659us

[13:30:42.872] KPI_DATA: [BOOTLOADER PROFILE] Sciclient Get Version : 9845us

[13:30:42.872] KPI_DATA: [BOOTLOADER PROFILE] CPU load : 81377us

[13:30:42.872] KPI_DATA: [BOOTLOADER PROFILE] SBL End : 3us

[13:30:42.872] KPI_DATA: [BOOTLOADER_PROFILE] SBL Total Time Taken : 606366us

[13:30:42.882]

[13:30:42.882] Image loading done, switching to application ...

[13:30:42.882] IO-Device V4.2.0.0, ID: 8f9b6f2f

[13:30:43.382] Restore remanent memory indicated.

[13:30:43.382] Using user-defined submodule configuration (not from remanent memory).

[13:30:43.392] Restore remanent memory indicated.

[13:30:43.392] Restore remanent memory indicated.

[13:30:43.402] Restore remanent memory indicated.

[13:30:43.402] Restore remanent memory indicated.

[13:30:43.402] Restore remanent memory indicated.

[13:30:43.412] [APP] INFO: Initializing PRU instance ...

[13:30:43.412] DP83869 detected

[13:30:43.412] DP83869 detected

[13:30:43.412] Phy 3 : Disable RGMII mode

[13:30:43.420] Phy 3 : Disable GBit ANEG

[13:30:43.420] Phy 15 : Disable RGMII mode

[13:30:43.420] Phy 15 : Disable GBit ANEG

[13:30:43.420] Module/submodule successfully plugged into slot 0, subslot 1

[13:30:43.452] Module/submodule successfully plugged into slot 0, subslot 2

[13:30:43.452] Module/submodule successfully plugged into slot 0, subslot 3

[13:30:43.462] Module/submodule successfully plugged into slot 0, subslot 4

[13:30:43.462] Module/submodule successfully plugged into slot 1, subslot 1

[13:30:43.473] Module/submodule successfully plugged into slot 1, subslot 2

[13:30:43.473] Module/submodule successfully plugged into slot 1, subslot 3

[13:30:43.480] Restore remanent memory indicated.

[13:30:43.480]

Hope to successfully conduct the Profinet test on the LP-AM2434.

Thanks

  • Hi Tan Bao,

    The UART console logs for application initialization seems to be correct,

    1) Could you use the PRONETA tool to confirm whether the AM243x-LP is detected?

    2) Also could you share the binaries used for flashing the application to test at our setup? Have you replaced the flashing binaries as shared in the patch?

    Regards,

    Laxman