This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Request: Technical Docs for Texas Instruments Compiler v18.1.3.LTS

Part Number: TMS570LC4357
Other Parts Discussed in Thread: ARM-CGT

Tool/software:

Hello,
I’m with Alta Rail Technology (Brazil), working on an SIL4 certification effort for a railway application. Our system uses a board from the Canadian supplier SC3 Automation (https://sc3automation.com/), and their design relies on the Texas Instruments compiler v18.1.3.LTS.

To advance our certification activities, could you please provide the following documents for this compiler version?

  • User Guide

  • Release Notes

  • Defect Coverage

We have previously signed an NDA with Texas Instruments for requesting documentation. If there is a specific process or portal we should use, please let me know.

Thank you,


Maicon M. Machado
Alta Rail Technology, Brazil
maicon.machado@alta-rt.com

  • All of the documentation for TI Arm compiler version 18.1.3.LTS is still available online.

    Start on the home page for TI Arm compilers.  Near ARM-CGT click on Download options.  Click on View all versions.  In the search box just under Select a version enter 18.1.3.  Click on 18.1.3.LTS.  The page that results contains ...

    • User Guide

    • Release Notes

    • Defect Coverage

    ... and more.

    Thanks and regards,

    -George

  • Hello George!

    Thank you for your response.

    I was able to download the documents, but the Release Notes link appears to be broken:

    https://downloads.ti.com/codegen/esd/cgt_public_sw/TMS470/18.1.3.LTS/README.txt

    Could you please verify and share an updated link, or attach the Release Notes directly?

    Thank you

  • I apologize for the problem.  I let the relevant team know.

    One way to access the readme is by installing the compiler.  It is located in the root directory of the installation.  For your convenience, I have also attached it below.

    Thanks and regards,

    -George

                           ARM C/C++ CODE GENERATION TOOLS
                               18.1.3.LTS Release Notes
                                      July 2018
    
    ================================================================================
    Contents
    ================================================================================
    1)  Support Information
    
    2)  New Features
    
    2.1) C++14 support
     
    * Features Included from v17.9.0.STS:
    2.2) C++ ABI Compatibility
    
    2.3) Support for ARM C Language Extensions (ACLE)
    
    * Features Included from v16.12.0.STS:
    2.4) Improved stack usage with inline functions
    
    
    -------------------------------------------------------------------------------
    1.  Support Information
    -------------------------------------------------------------------------------
    
    -------------------------------------------------------------------------------
    1.1) List of Fixed and Known Defects
    -------------------------------------------------------------------------------
    
    As of the 16.12.0.STS release, the DefectHistory.txt file has been replaced
    with the two files Open_defects.html and Closed_defects.html. For open bugs, a
    status of Open or Accepted means that the bug has not been examined yet,
    whereas a status of Planned means that an evaluation or fix is in progress.
    
    -------------------------------------------------------------------------------
    1.2) Compiler Wiki
    -------------------------------------------------------------------------------
    
    A Wiki has been established to assist developers in using TI Embedded
    Processor Software and Tools.  Developers are encouraged to read and
    contribute to the articles.  Registered users can update missing or
    incorrect information.  There is a large section of compiler-related
    material.  Please visit:
    
    http://processors.wiki.ti.com/index.php?title=Category:Compiler
    
    -------------------------------------------------------------------------------
    1.3) Compiler Documentation Errata
    -------------------------------------------------------------------------------
    
    Errata for the "TI ARM Optimizing Compiler User's Guide" and the
    "TI ARM Assembly Language User's Guide" is available online at the
    Texas Instruments Embedded Processors CG Wiki:
    
    http://processors.wiki.ti.com/index.php?title=Category:Compiler
    
    under the 'Compiler Documentation Errata' link.
    
    -------------------------------------------------------------------------------
    1.4) TI E2E Community
    -------------------------------------------------------------------------------
    
    Questions concerning TI Code Generation Tools can be posted to the TI E2E
    Community forums.  The "Development Tools" forum can be found at:
    
    http://e2e.ti.com/support/development_tools/f/default.aspx
    
    -------------------------------------------------------------------------------
    1.5) Defect Tracking Database
    -------------------------------------------------------------------------------
    
    Compiler defect reports can be tracked at the Development Tools bug
    database, SDOWP. The log in page for SDOWP, as well as a link to create
    an account with the defect tracking database is found at:
    
    https://cqweb.ext.ti.com/pages/SDO-Web.html
    
    A my.ti.com account is required to access this page.  To find an issue
    in SDOWP, enter your bug id in the "Find Record ID" box once logged in.
    To find tables of all compiler issues click the queries under the folder:
    
    "Public Queries" -> "Development Tools" -> "TI C-C++ Compiler"
    
    With your SDOWP account you can save your own queries in your
    "Personal Queries" folder.
    
    -------------------------------------------------------------------------------
    1.6) Long Term Support release
    -------------------------------------------------------------------------------
    The ARM CGT v18.1.0.LTS release is a long term support (LTS) release. This
    release will be supported for roughly 2 years with periodic bug fix updates.
    
    
    -------------------------------------------------------------------------------
    2. New Features
    -------------------------------------------------------------------------------
    
    --------------------------------------------------------------------------------
    2.1) C++ 2014 RTS support
    --------------------------------------------------------------------------------
    
    As of v18.1.0.LTS, the compiler uses the C++14 version of the C++ standard. 
    Previously, C++03 was used. See the C++ Standard ISO/IEC 14882:2014. For a 
    description of unsupported C++14 features, see Section 5.2 of the "TI ARM
    Optimizing Compiler User's Guide".
    
    The move to C++14 will break ABI compatibility with previous C++ RTS releases. 
    Attempting to link old C++ object code with the new RTS will result in a 
    link-time error. Suppressing this error will likely result in undefined symbols 
    or undefined behavior during execution. 
    
    C ABI compatibility will not be affected by this change.
    
    In most cases, recompiling old source code with the new RTS should be safe.
    However, due to the changes made in the language, some constructs will result
    in syntax errors. Some common issues include:
    - Macro expansion immediately adjacent to string literals may fail due to the
      inclusion of new string literals and literal suffixes.
      Ex: u8"def" will fail to compile if 'u8' is a macro
          "def"_x will fail to compile if '_x' is a macro
    - New keywords: alignas, alignof, char16_t, char32_t, constexpr, decltype,
      noexcept, nullptr, static_assert, and thread_local
    - The auto keyword has been repurposed and is no longer a valid storage class
      specifier. Similarly, the register keyword has been deprecated and will be
      removed in the future.
    
    A full list can be found in Appendix C, section 2 of the C++14 standard.
    
    -------------------------------------------------------------------------------
    2.2) C++ ABI Compatibility
    -------------------------------------------------------------------------------
    
    v17.9.0.STS contains the first planned updates in preparation for the support
    of C++14 (International Standard ISO/IEC 14882:2014(E)). As part of this
    update, it is necessary to make changes which might cause errors when building
    C++ projects containing C++ object files compiled with older versions of the
    compiler.
    
    These errors will usually include linktime errors involving undefined symbols.
    If you see undefined symbol errors during a link, pass the "--no_demangle"
    option to the compiler. If the undefined symbol's name starts with _Z or _ZVT,
    then it's possible that there is a C++ object file or library built with an
    older version of the tools being used. These will need to be compiled with the
    v18.1.0.LTS tools to work properly.
    
    
    -------------------------------------------------------------------------------
    2.3) Support for ARM C Language Extensions (ACLE)
    -------------------------------------------------------------------------------
    
    Beginning with the ARM CGT v17.9.0.STS release, support for ARM C Language
    Extensions (ACLE) as specified in the ACLE Release 2.0 document (Document
    number: IHI 0053C, Date of Issue: 09/05/2014) has been added for the
    applicable processor variants that are supported in the ARM CGT. This includes
    support for new ACLE attributes, intrinsics, and pre-defined symbols as
    detailed in the sub-sections below.
    
    
    2.2.1) ACLE Attributes
    ----------------------
    
    In addition to the attributes described in the ACLE specification that the
    ARM CGT already supports (i.e. aligned, alias, common, nocommon, packed, 
    section, visibility, and weak), the ARM CGT v17.9.0.STS release adds support
    for the "target" attribute as follows:
    
      __attribute__((target("arm"))) void myfunc()
      
         when applied to a function, will force the generation of ARM state code. 
         This attribute will be interpreted as if the user had specified the
         already supported "#pragma CODE_STATE(myfunc, 32)" just in front of the
         definition of the function definition of "myfunc".
    
      __attribute__((target("thumb"))) void myfunc()
      
         when applied to a function, will force the generation of THUMB state code. 
         This attribute will be interpreted as if the user had specified the
         already supported "#pragma CODE_STATE(myfunc, 16)" just in front of the
         definition of the function definition of "myfunc".
    
    The ARM CGT does not support the "pcs" ACLE attribute.
    
    
    2.2.2) ACLE Intrinsics
    ----------------------
    
    A new header file, arm_acle.h, has been added to the ARM CGT include
    subdirectory which provides declarations and/or declarations of all of the
    ACLE intrinsics that are now supported beginning with the v17.9.0.STS 
    release.
    
    The majority of ACLE intrinsics that are newly supported in this release
    are implemented by already supported intrinsics that may have a slightly
    different name. For example, the ACLE "__smulbb" intrinsic is implemented 
    in terms of the already supported "_smulbb" intrinsic as follows:
    
      int32_t __BUILTIN _smulbb(int32_t x, int32_t y);
      #define __smulbb  _smulbb
    
    The only difference being that the ACLE "__smulbb" intrinsic name has
    a prefix of two underscores as opposed to the name of the already
    supported "_smulbb" intrinsic name which has a prefix of 1 underscore.
    
    The ARM CGT v17.9.0.STS release does not support all of the ACLE intrinsics
    that are included in the ACLE specification. For example, the __cls, __clsl,
    and __clsll ACLE intrinsics are not supported since the CLS instruction is
    not available on the Cortex-M or Cortex-R architectures.
    
    Please see the arm_acle.h file for more details about exactly which ACLE
    intrinsics are supported and which are not. Where applicable, the declarations
    of ACLE intrinsics that are not supported are enclosed in comments along with
    a brief explanation of why the intrinsic is not supported and a reference to
    the appropriate section in the ACLE specification where the intrinsic is
    described.
    
    
    2.2.3) ACLE Pre-Defined Symbols
    -------------------------------
    
    The ARM CGT v17.9.0.STS compiler will now define the following ACLE 
    pre-defined symbols:
    
    __ARM_ACLE		  - defined to '200' for all Cortex-M and Cortex-R
    			    processor variants supported by the ARM CGT, not
    			    defined otherwise
    
    __ARM_ARCH		  - indicates which ARM architecture the compiler
    			    is generating code for:
    			  
    			    value	selected processor
    			    -----	------------------
    			    '4'	-mv4
    			    '5'	-mv5e
    			    '6'	-mv6, -mv6m0
    			    '7'	-mv7a8, -mv7m3, -mv7m4, -mv7r4, -mv7r5
    			 
    __ARM_32BIT_STATE	  - defined to 1 if compiler is generating code for
    			    an ARM 32-bit processor variant, otherwise
    			    undefined
    
    __ARM_ARCH_ISA_ARM	  - defined to 1 if compiler is generating code for
    			    a processor variant that supports the ARM 
    			    instruction set; otherwise undefined (not
    			    defined when compiling for Cortex-M processor,
    			    for example)
    
    __ARM_ARCH_ISA_THUMB	  - defined to 1 if compiler is generating code for
    			    a processor variant that supports the THUMB-1
    			    instruction set; defined to 2 if compiler is 
    			    generating code for a processor variant that 
    			    supports the THUMB-2 instruction set; otherwise
    			    undefined
    
    __ARM_BIG_ENDIAN	  - matches endian-ness specified with compiler
    			    command-line: 1 (big-endian; default), 
    			    0 (little-endian; -me option)
    
    __ARM_FEATURE_CLZ	  - defined to 1 if compiler is generating code for
                                a processor variant that supports the CLZ 
    			    instruction; otherwise undefined
    
    __ARM_FEATURE_DSP	  - defined to 1 if compiler is generating code for
    			    a Cortex-M or Cortex-R processor that supports
    			    DSP instructions/intrinsics; otherwise undefined
    
    __ARM_FEATURE_SAT	  - defined to 1 if compiler is generating code for
    			    a processor variant tha supports SSAT/USAT 
    			    instructions/intrinsics; otherwise undefined
    
    __ARM_FEATURE_SIMD32 	  - defined to 1 if compiler is generating code for
    			    a processor variant that supports all SIMD
    			    instructions/intrinsics; otherwise undefined
    
    __ARM_FEATURE_UNALIGNED   - defined to 1 if compiler is generating code for
    			    a processor variant that supports unaligned access
    			    to memory; otherwise undefined
    
    __ARM_PCS		  - defined to 1 if the compiler can assumes that
    			    the default procesude calling standard for a 
    			    translation unit conforms to the "base procedure
    			    call standard" as prescribed in the ARM 
    			    Architecture Procedure Call Standard specification;
    			    otherwise undefined
    
    __ARM_SIZEOF_MINIMAL_ENUM - smallest possible enum type size (1 byte
    			    for 'packed', 4 bytes for 'int' (mirroring the
    			    --enum_type=[packed|int] option where packed is
    			    the default)
    
    __ARM_SIZEOF_WCHAR_T	  - size of wchar_t type: 16- (default) or 32-bits
    
    __ARM_FP		  - defined to a non-zero value if the compiler can
    			    assume that floating-point hardware support is
    			    available when compiling a translation unit. The
    			    value will be a combination of:
    
    			    bit  value  precision
                                ---  -----  ---------
    			     1    0x2    16-bit
    			     2    0x4    32-bit
    			     3    0x8    64-bit
    
    			    For example, if --float_support=fpv4spd16 is
    			    selected, then __ARM_FP will have a value of
    			    0x6 since fpv4spd16 supports 32-bit and 16-bit
    			    floating-point hardware.
    
    			    If no floating-point hardware support is enabled,
    			    then __ARM_FP will be undefined.
    
    __ARM_FP16_ARGS		  - defined to 1 if a 16-bit float type can be used
    			    for an argument and/or result; otherwise undefined
    
    __ARM_FP16_FORMAT_IEEE	  - defined to 1 if the IEEE format for 16-bit
    			    floating-point (according to IEEE 754-2008
    			    standard) is used; otherwise undefined
    
    __ARM_PCS_VFP		  - defined to 1 if the default procedure calling 
    			    convention is to pass floating-point arguments /
    			    return values in hardware floating-point 
    			    registers
    
    The ARM CGT v17.9.0.STS release does not support all of the ACLE pre-defined
    symbols that are included in the ACLE specification. For example, the 
    __ARM_FEATURE_CRYPTO pre-defined symbol is associated with support for 
    CRYPTO instructions which are not supported on any of the processor variants
    that the ARM CGT v17.9.0.STS release supports. If an ACLE pre-defined symbol
    in the ACLE specification is not included in the above list, then it will
    not be defined by the ARM CGT compiler.
    
    
    -------------------------------------------------------------------------------
    2.4) Improved stack usage with inline functions
    -------------------------------------------------------------------------------
    
    The new compiler improves stack usage by sharing aggregate data originally
    defined in inline functions. Example:
    
    struct ARGS { int f1,f2,f3,f4,f5; };
    
    static inline void func1()
    {
       struct ARGS a = {1, 2, 3, 4, 5};
       foo(&a);
    }
    
    static inline void func2()
    {
       struct ARGS b = {1, 2, 3, 4, 5};
       foo(&b);
    }
    
    void func3()
    {
       func1();
       func2();
    }
    
    
    In previous compilers, if func1 and func2 are inlined, the structs a
    and b would not share the same stack location. This version of the
    compiler will now share stack memory for local aggregates defined in
    inline functions.