Part Number: AM2634
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi Ti Family,
We have designed new board based on AM2634 MCU and to connect and load the program we are using XDS110 debug probe.
I am currently debugging and running program on MCU using DEV Boot or No Boot mode.
I need clarification on " can i flash the code using the same boot ( No Boot) mode?".
or
Do I need to flash the code first and change the boot mode later on so that it load the program from RAM?
Thanks and Regards