Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello,
I have a project which uses the Timer0 to trigger ADC conversion. The Timer0 period is set as 1.125s while the Timer clock frequency as 3.64KHz.
The event publisher is Timer0 and the event subscriber is ADC12_0. The conversion occurs every 100us. But I couldn't find where 100us is configured in the SysCfg.
Here is the ADC12_0 init function in ti_msp_dl_config.c:
SYSCONFIG_WEAK void SYSCFG_DL_ADC12_0_init(void)
{
DL_ADC12_setClockConfig(ADC12_0_INST, (DL_ADC12_ClockConfig *) &gADC12_0ClockConfig);
DL_ADC12_initSeqSample(ADC12_0_INST,
DL_ADC12_REPEAT_MODE_ENABLED, DL_ADC12_SAMPLING_SOURCE_AUTO, DL_ADC12_TRIG_SRC_EVENT,
DL_ADC12_SEQ_START_ADDR_00, DL_ADC12_SEQ_END_ADDR_03, DL_ADC12_SAMP_CONV_RES_12_BIT,
DL_ADC12_SAMP_CONV_DATA_FORMAT_UNSIGNED);
DL_ADC12_configConversionMem(ADC12_0_INST, ADC12_0_ADCMEM_2,
DL_ADC12_INPUT_CHAN_2, DL_ADC12_REFERENCE_VOLTAGE_VDDA, DL_ADC12_SAMPLE_TIMER_SOURCE_SCOMP0, DL_ADC12_AVERAGING_MODE_DISABLED,
DL_ADC12_BURN_OUT_SOURCE_DISABLED, DL_ADC12_TRIGGER_MODE_AUTO_NEXT, DL_ADC12_WINDOWS_COMP_MODE_DISABLED);
DL_ADC12_configConversionMem(ADC12_0_INST, ADC12_0_ADCMEM_3,
DL_ADC12_INPUT_CHAN_3, DL_ADC12_REFERENCE_VOLTAGE_VDDA, DL_ADC12_SAMPLE_TIMER_SOURCE_SCOMP0, DL_ADC12_AVERAGING_MODE_DISABLED,
DL_ADC12_BURN_OUT_SOURCE_DISABLED, DL_ADC12_TRIGGER_MODE_AUTO_NEXT, DL_ADC12_WINDOWS_COMP_MODE_DISABLED);
DL_ADC12_setPowerDownMode(ADC12_0_INST,DL_ADC12_POWER_DOWN_MODE_MANUAL);
DL_ADC12_setSampleTime0(ADC12_0_INST,20);
DL_ADC12_setSampleTime1(ADC12_0_INST,50);
DL_ADC12_setSubscriberChanID(ADC12_0_INST,ADC12_0_INST_SUB_CH);
/* Enable ADC12 interrupt */
DL_ADC12_clearInterruptStatus(ADC12_0_INST,(DL_ADC12_INTERRUPT_MEM2_RESULT_LOADED
| DL_ADC12_INTERRUPT_MEM3_RESULT_LOADED));
DL_ADC12_enableInterrupt(ADC12_0_INST,(DL_ADC12_INTERRUPT_MEM2_RESULT_LOADED
| DL_ADC12_INTERRUPT_MEM3_RESULT_LOADED));
DL_ADC12_enableConversions(ADC12_0_INST);
}
Here is the Timer0 init function in ti_msp_dl_config.c:
SYSCONFIG_WEAK void SYSCFG_DL_TIMER_0_init(void) {
DL_TimerG_setClockConfig(TIMER_0_INST,
(DL_TimerG_ClockConfig *) &gTIMER_0ClockConfig);
DL_TimerG_initTimerMode(TIMER_0_INST,
(DL_TimerG_TimerConfig *) &gTIMER_0TimerConfig);
DL_TimerG_enableClock(TIMER_0_INST);
DL_TimerG_enableEvent(TIMER_0_INST, DL_TIMERG_EVENT_ROUTE_1, (DL_TIMERG_EVENT_ZERO_EVENT));
DL_TimerG_setPublisherChanID(TIMER_0_INST, DL_TIMERG_PUBLISHER_INDEX_0, TIMER_0_INST_PUB_0_CH);
}
I guess it must be somewhere I missed. Can you help with this?
Thanks!
Crane