Part Number: MSPM0G1519
Tool/software:
Champs,
I was under impression that issuing "System Reset" from CCS Run menu is expected to trigger reset pulse on the NRST pin of the MCU. I tested it using LED blink example by reducing the DELAY to 16 core cycles making it appear permanently lit and then issuing the system reset expecting a short LED off interval while the MCU goes through reset. this did not happen. The Launchpad is in factory state, NRST jumper between xds110 and the MCU is installed. will appreciate your clarification if this is expected to work
thanks
Michael