Part Number: LP-AM243
Other Parts Discussed in Thread: SYSCONFIG, , AM2434
Tool/software:


Hi TI support team,
Would you tell me which SysConfig version and Variant is suitable for our environment?
I am using LP-AM243 board.
OPN#: LP-AM243
PCB#: PROC109A(001)
From the board infomation below
proc109a_sch
I think the board has "XAM2434BSFGHIALX."
And I have confirmed the markings on the CPU was "AM2434B."
I will also use "MOTOR CONTROL SDK for AM243x Ver. 9.2.0.09" for my development.
When I set "SysConfig 1.23.0", then showing example.syscfg on Code Composer Studio 20.2.0.12,
I can only choose following in Select Device dialog.
---------------
Select Device
Device: AM2434
Package: FCCSP (ALX)
---------------
When I set "SysConfig 1.24.0", then showing example.syscfg on Code Composer Studio 20.2.0.12,
I have 3 Variant alternatives in Select Device dialog.
----------------------
Select Device
Device: AM2434
Package: FCCSP (ALX)
Variant: AM2434-E / AM2434-F / AM24324-D
----------------------
If I could find AM2434-B in Variant, I would use it. But Revision-B is not shown.
Which is better using SysConfig 1.23.0 or 1.24.0?
In case I will use 1.24.0, what variant should I use?
Thanks in advance.
Best regards,
Dai