This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Handling unused pins



Is there a document listing the recommended approach for all the 144 pins if some of them are not used? Thanks.

Regards,

Yashas

  • No. We don't have such a document now. For most of the digital pins, they have internal pull up/down, you can leave them open. Unused FlexRay pins can be left open as well. ADC pins can left open too. Test pin should connect to ground. nRST is better to have a external pull up(1-10k) and filter cap (around 100pF). NPORRST should have a external pull up (1-3k) and filter cap (around 100pF).

    If you are not sure about a certain pin, please post them.

    Regards,

    Haixiao