AM263P4: post processing setup for Code Computer Studio after Linker is finished building target .out file

Part Number: AM263P4

Tool/software:

In the gpio_led_blink example project in mcu_plus_sdk_am263px_10_02_00_15, where the project settings are setup in CCS 12.8 GUI in order to run following post linker commands?

How can I setup the ARM core to execute at the maximum speed of 400MHz.  I could not find setting the core speed in syscfg.

Thanks for your help.

*************************  post linker processing *****************************

Finished building target: "gpio_led_blink.out"

C:/Users/214008820/ti/ccs/utils/bin/gmake -C C:\Users\214008820\Documents\AM263P4_Projects3\gpio_led_blink -f makefile_ccs_bootimage_gen OUTNAME=gpio_led_blink PROFILE=Debug MCU_PLUS_SDK_PATH=C:/Users/214008820/ti/mcu_plus_sdk_am263px_10_02_00_15 CG_TOOL_ROOT=C:/Users/214008820/ti/ccs/tools/compiler/ti-cgt-armllvm_4.0.1.LTS CCS_INSTALL_DIR=C:\Users\214008820\ti\ccs CCS_IDE_MODE=desktop DEVICE=am263px
Boot image: am263px:r5fss0-0:nortos:ti-arm-clang C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.appimage ...
C:\Users\214008820\ti\ccs/tools/node/node C:/Users/214008820/ti/mcu_plus_sdk_am263px_10_02_00_15/tools/boot/out2rprc/elf2rprc.js Debug/gpio_led_blink.out >> Debug/temp_stdout_Debug.txt
C:\Users\214008820\ti\ccs/utils/cygwin/cp gpio_led_blink.rprc C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.rprc
C:\Users\214008820\ti\ccs/utils/cygwin/cp C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.rprc C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.rprc_tmp
C:\Users\214008820\ti\ccs/utils/cygwin/rm -f C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.rprc
C:/Users/214008820/ti/mcu_plus_sdk_am263px_10_02_00_15/tools/boot/xipGen/xipGen.exe -i C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.rprc_tmp -o C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.rprc -x C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.rprc_xip --flash-start-addr 0x60000000 -v > Debug/temp_stdout_Debug.txt
C:\Users\214008820\ti\ccs/tools/node/node C:/Users/214008820/ti/mcu_plus_sdk_am263px_10_02_00_15/tools/boot/multicoreImageGen/multicoreImageGen.js --devID 55 --out C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.appimage C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.rprc@0 >> Debug/temp_stdout_Debug.txt
C:\Users\214008820\ti\ccs/tools/node/node C:/Users/214008820/ti/mcu_plus_sdk_am263px_10_02_00_15/tools/boot/multicoreImageGen/multicoreImageGen.js --devID 55 --out C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.appimage_xip C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.rprc_xip@0 >> Debug/temp_stdout_Debug.txt
C:\Users\214008820\ti\ccs/utils/cygwin/rm -f C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.rprc_tmp
Boot multi-core ELF image: am263px:r5fss0-0:nortos:ti-arm-clang C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.mcelf ...
python C:/Users/214008820/ti/mcu_plus_sdk_am263px_10_02_00_15/tools/boot/multicore-elf/genimage.py --core-img=0:Debug/gpio_led_blink.out --output=C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.mcelf --merge-segments=true --tolerance-limit=0 --ignore-context=false --xip=0x60000000:0x68000000 --xlat=none --max-segment-size=8192
Boot multi-core ELF image: C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.mcelf Done !!!
.
Boot image: am263px:r5fss0-0:nortos:ti-arm-clang C:/Users/214008820/Documents/AM263P4_Projects3/gpio_led_blink/Debug/gpio_led_blink.appimage Done !!!
.

**** Build Finished ****