Part Number: SYSCONFIG
Other Parts Discussed in Thread: SHA-256
Tool/software:
Hello,
I recently installed the latest Sysconfig (1.24.2) in my Windows 10 machine. I'm not able to start the GUI, either by using the shortcut or by calling the sysconfig_gui.bat file. If I call the sysconfig_gui.bat file from the command line, I dont see any error. On the contrary, I can use the cli bat file and generate the files with it, but it I need the GUI.
I rebooted the machine, reinstall it again and so on, without success. Apart from that, I have no issues with the previous sysconfig versions, its only with the latest.
I had a look in the install log files but I didnt find any issue either. The file is not corrupt, SHA-256 is the same.
Any ideas?
Thanks in advance,
Álvaro