This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: EPWM sync to IEP (SDFM, Endat) sporadically not working

Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

Hello everyone,

Over the past few days, I’ve been debugging a tricky and sporadic issue that I’d like to share—hopefully it saves someone else some time if they encounter the same problem.

My setup:

  • EPWM0–2 used for motor PWM
  • SDFM and EnDat running on ICSSG0
  • Periodic sampling triggered by IEP0 compare events
  • IEP0 is intended to be synchronized with EPWM0, so I disabled the periodic reset of IEP0 via CMP1

The problem: After boot-up, the SDFM and EnDat sampling either worked perfectly or didn’t work at all. I discovered that in the non-working case, IEP0 was never reset by the EPWM sync-out event—even though all configuration registers for EPWM and IEP were identical to the working case.

Interestingly, I could get it working again by manually triggering a software sync-in on EPWM0.

The root cause: EPWM was running at 250 MHz, while IEP0 was set to the sysconfig default of 200 MHz. I suspect the EPWM sync-out signal isn’t properly latched or synchronized by IEP0, causing it to miss every 5th sync event due to the frequency mismatch.

So, depending on whether the sync-out event happens to fall into this “blind spot” during boot-up, the synchronization may fail.

The solution: Increase the IEP0 frequency to ≥ EPWM frequency. This ensures that IEP0 can reliably detect the sync-out events.

Ideally, this condition should be enforced by sysconfig or validated by the SDFM drivers.

Best regards,
Stefan