Part Number: LP-MSPM0C1104
Other Parts Discussed in Thread: MSPM0C1104, MSPM0L1306
Tool/software:
i download the example of uart_rw_multibyte_fifo_poll_LP_MSPM0C1104_nortos_ticlang
can print at UART with 4 words, "MSP!"
and if i have a float variable,
is there any way i can print at UART?
just like below code.
include <stdio.h>
int main(){
uint8_t correct_word[4] = {'M', 'S', 'P', '!'};
DL_UART_Main_fillTXFIFO(UART_0_INST, &correct_word[0], 4);
while (DL_UART_Main_isBusy(UART_0_INST))
;
// previous is work correctly, show the "MSP!" correct
// below will be compile ok, but nothing show at UART.
float tmp =23.6f;
char buffer[50]={0};
sprintf(buffer, "%4.1f", tmp);
DL_UART_Main_fillTXFIFO(UART_0_INST, &buffer[0], 4);
while (DL_UART_Main_isBusy(UART_0_INST))
;
}
as i know, maybe i need something like FTOA function or need compile with float support or else,
is there any hints can provide to me?